Skip to main content
Associate III
December 4, 2024
Solved

BLE_p2pServer build fail with NUCLEO-WBA55CG board

  • December 4, 2024
  • 1 reply
  • 2747 views

Hi Sir,

I run BLE_p2pServer example code with NUCLEO-WBA55CG board, it shows build error on STM32CubeIDE. How to fix it ?

Kenwang_0-1733294771016.png

The software version I used is :
STM32CubeIDE 1.17.0

STM32Cube_FW_WBA_V1.5.0

STM32CubeMX 6.13.0

This topic has been closed for replies.
Best answer by STTwo-32

Hello @Kenwang 

I'm able to reproduce this behavior using STM32CubeIDE 1.17.0, STM32Cube_FW_WBA_V1.5.0 and STM32CubeMX 6.13.0 and I've escalated for correction on the coming releases (under internal ticket number 197703). 

As a temporary workaround, could you please go to \STM32Cube_FW_WBA_V1.5.0\Projects\NUCLEO-WBA55CG\Applications\BLE\BLE_p2pServer\STM32CubeIDE and open the .cproject file. That should work fine. or go to File\Open Projects from file System... and select \STM32Cube_FW_WBA_V1.5.0\Projects\NUCLEO-WBA55CG\Applications\BLE\BLE_p2pServer\STM32CubeIDE on the Import source Directory and click on finish.

Best Regards.

STTwo-32

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
December 4, 2024

Hello @Kenwang 

I'm able to reproduce this behavior using STM32CubeIDE 1.17.0, STM32Cube_FW_WBA_V1.5.0 and STM32CubeMX 6.13.0 and I've escalated for correction on the coming releases (under internal ticket number 197703). 

As a temporary workaround, could you please go to \STM32Cube_FW_WBA_V1.5.0\Projects\NUCLEO-WBA55CG\Applications\BLE\BLE_p2pServer\STM32CubeIDE and open the .cproject file. That should work fine. or go to File\Open Projects from file System... and select \STM32Cube_FW_WBA_V1.5.0\Projects\NUCLEO-WBA55CG\Applications\BLE\BLE_p2pServer\STM32CubeIDE on the Import source Directory and click on finish.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KenwangAuthor
Associate III
December 6, 2024

By the way, if the IDE uses IAR, errors will still occur, but the error symptoms are different. I hope this problem can be improved in the next version, thank you.

Kenwang_0-1733446741854.png