Skip to main content
HSing
Associate II
July 24, 2019
Question

After the new firmware package for STM32WB, v1.2, I am not able to see the STM32WB on COM port after running a simple USB CDC code to enable serial communication.

  • July 24, 2019
  • 2 replies
  • 815 views
//main.c file
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_device.h"
#include "gpio.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "usbd_cdc_if.h"
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
extern USBD_HandleTypeDef hUsbDeviceFS;
//extern uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len);
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USB_Device_Init();
 /* USER CODE BEGIN 2 */
 char dataOut[256];
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
	
	 sprintf(dataOut, "HelloWorld");
	 //CDC_Transmit_FS(( uint8_t * )dataOut, strlen( dataOut ));
	 USBD_CDC_SetTxBuffer(&hUsbDeviceFS, ( uint8_t * )dataOut, strlen( dataOut ));
	 USBD_CDC_TransmitPacket(&hUsbDeviceFS);
	 HAL_Delay(1000);
 }
 /* USER CODE END 3 */
}

The mentioned code should send "HelloWorld" every second over USB. I have connected both the USBs to STM32WB. I able to see one port which is used to for debugging/downloading but can't see the other one. Anyone with any idea?

This topic has been closed for replies.

2 replies

LVent
Associate II
August 6, 2019

Yes, there is an issue in the code generation with this package version.

Try to add 0x00 in the third position in the declaration of USBD_CDC_DeviceDesc in usbd__desc.c file.

ST Employee
August 14, 2019

Hi,

Why not checking the CDC example provided in STM32WBCube package first and then compare it with your generated code ?

If you use one of ST boards (ie. Nucleo or Dongle) then the application would work straight forward.

Basically what you need to check first place is:

  • USB clock source (normally it should be CRS, so check that CRS is running and configured correctly and that USB is using it as source clock)
  • USB dedicated VDD IO shall be connected to 3.3V on the board
  • USB interruption is configured correctly and with right priority

I hope it helps.