2020-05-15 10:30 AM
Hello - My project is based on the SensorDemoBLESensor application built using using the CubeMX tool version 5.6.1 with the X-NUCLEO-BNRG2A1 development board attached to a NUCLEO-F303RE. I successfully added 5 custom characteristics to my first custom service. When I attempt to add a 6th characteristic the aci_gatt_add_char() returned 0x48 (BLE_STATUS_OUT_OF_MEMORY) on the STM32F303. I added a 2nd custom service and successfully added the characteristic that failed to add on the first service. So I don't think this a total memory problem.
The modified the default DTM settings in DTM_Config.h running on the BlueNRG-M2 as follows:
#define DTM_NUM_LINK 2 // Was 8
#define DTM_NUM_GATT_SERVICES 5 // Was 8
#define DTM_NUM_GATT_ATTRIBUTES 125 // Was 68
#define ATT_VALUE_ARRAY_SIZE (3000) // Was 1248
I still see the error. There seems to be a limit to the number of characteristics (attributes) per service.
Any help would be appreciated.
Best
Solved! Go to Solution.
2020-05-21 1:59 AM
Hello,
when adding a characteristic to a service you should verify that, when creating that service using the function aci_gatt_add_service(), you declared a sufficient number of attribute records.
For instance, in the SensorDemo_BLESensor-App, in function Add_HWServW2ST_Service() you have:
/* Add_HWServW2ST_Service */
COPY_HW_SENS_W2ST_SERVICE_UUID(uuid);
BLUENRG_memcpy(&service_uuid.Service_UUID_128, uuid, 16);
ret = aci_gatt_add_service(UUID_TYPE_128, &service_uuid, PRIMARY_SERVICE,
1+3*5, &HWServW2STHandle);
if (ret != BLE_STATUS_SUCCESS)
return BLE_STATUS_ERROR;where (1+3*5) is the Max_Attribute_Records, i.e. the Maximum number of attribute records that can be added to this service.
In such a case you can have no more than 5 characteristics (all readable, writable and notify).
If you need to have 6 characteristics, you have to increase the Max_Attribute_Records value to (1+3*6).
BR
Silvio
2020-05-21 1:59 AM
Hello,
when adding a characteristic to a service you should verify that, when creating that service using the function aci_gatt_add_service(), you declared a sufficient number of attribute records.
For instance, in the SensorDemo_BLESensor-App, in function Add_HWServW2ST_Service() you have:
/* Add_HWServW2ST_Service */
COPY_HW_SENS_W2ST_SERVICE_UUID(uuid);
BLUENRG_memcpy(&service_uuid.Service_UUID_128, uuid, 16);
ret = aci_gatt_add_service(UUID_TYPE_128, &service_uuid, PRIMARY_SERVICE,
1+3*5, &HWServW2STHandle);
if (ret != BLE_STATUS_SUCCESS)
return BLE_STATUS_ERROR;where (1+3*5) is the Max_Attribute_Records, i.e. the Maximum number of attribute records that can be added to this service.
In such a case you can have no more than 5 characteristics (all readable, writable and notify).
If you need to have 6 characteristics, you have to increase the Max_Attribute_Records value to (1+3*6).
BR
Silvio
2020-05-21 9:59 AM
Hello Silvio,
This solved my problem. Thank you for your time and effort.
BR
Dave
2020-06-16 12:55 PM
Can someone explain why a field labeled "Max_Attribute_ Records" should be "1+3*X"? What is the "1+3*" and why is it used? I used "6" and was able to add 2 characteristics to my service without issue, but fail on adding a 3rd. In terms of the documentation you would assume that supplying "6" would mean the service should support 6.
2020-06-27 2:55 AM
Hello,
this discussion thread can provide you with more information:
https://community.st.com/s/question/0D50X00009XkYAvSAN/sensortile-bluenrgms-custom-service-aci
BR
Silvio