Skip to main content
Associate III
Oct 22, 2024 4:52 PM UTC
Solved

TouchGFX keyboard with password

Hello to all,I am working on a stm32h745i-disk project that uses keyboard and I would like to hide the characters in the password field.

how can I do it? i.e. I don't understand when you press a key on the keyboard where do you type so that it is shown above the keyboard before you hit ok and it is passed to the GUI with “Unicode::strncpy(ContrasenaBuffer, keyboard.getBuffer(), CONTRASENA_SIZE);”

The video guide I used was:

https://www.youtube.com/watch?v=Tkz9099a7a4

testing and trying to understand the keyboard related files I could only hide them once you hit ok and they show up in the GUI using two buffers where one is filled with “*”.

 

I would like to do something similar to the video (minute 5:38) https://www.youtube.com/watch?v=0--7qFmWZMQ

but in my touchGFX code and later add a button to show the password if I want to but I guess I can do that later if I can solve this.

 

I share my View.cpp and the keyboard thing.please ignore Login_inicioView::Validacion_usuario() as it is something for the future.

Thanks.

 

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Oct 29, 2024 10:41 AM UTC

Hello @Maximiliano ,

 

By changing, in the CustomKeyboard.cpp file, the function KeyPressHandler

 

void CustomKeyboard::keyPressedhandler(Unicode::UnicodeChar keyChar)
{
 // Replace the actual key character with '*'
 keyChar = '*';

 // Add the '*' character to the buffer
 uint16_t pos = keyboard.getBufferPosition()-1;
 if (pos < BUFFER_SIZE - 1)
 {
 buffer[pos] = keyChar;
 keyboard.setBufferPosition(pos + 1);
 }
}

 

I am able to only display *.
However, I do that by replacing all the data in the buffer by *.
This means that you should create a new buffer to store the key you pressed.
I do that because the data in the buffer are displayed it is easier to change the buffer value than to change the code in Keyboard.hpp, also Keyboard.hpp is in widget, so I think it is regenerated every time so you cannot modify it.


Now what you have left to do is to create a new buffer in the customKeyboard files, store the key press in this buffer such as follow :

void CustomKeyboard::keyPressedhandler(Unicode::UnicodeChar keyChar)
{
 //Save data in new buffer
 myOwnBuffer += keyChar;
 
 // Replace the actual key character with '*'
 keyChar = '*';

 // Add the '*' character to the buffer
 uint16_t pos = keyboard.getBufferPosition()-1;
 if (pos < BUFFER_SIZE - 1)
 {
 buffer[pos] = keyChar;
 keyboard.setBufferPosition(pos + 1);
 }
}

Then you also have to change the getBuffer and clearBuffer functions that were added by the youtuber.

 

Hope this helps! :smiling_face_with_smiling_eyes:
If this comment answers your question, I invite you to select it as "best answer".

 

Regards

Gaetan GodartSoftware engineer at ST (TouchGFX)

16 replies

GaetanGodart
ST Employee
Oct 25, 2024 10:02 AM UTC

Hello @Maximiliano ,

 

What keyboard are you using?

In the keyboards people shared in the custom widget thread, there is usually a buffer inside the custom keyboard that stores the data and then we can access a method to return that data.
Usually, people just copy the buffer into a wildcard but you can just make another buffer to be displayed and keep the data secret.
Your displayed buffer should be only '*' except the last one.
Here is a function that would do that :

void transformText(const char* input, char* output)
{
 const char* p = input;
 char* q = output;
 
 // Find the length of the input manually
 size_t len = 0;
 while (input[len] != '\0') len++;
 
 if (len == 0)
 {
 output[0] = '\0';
 return;
 }
 
 // Replace all characters except the last one with '*'
 for (size_t i = 0; i < len - 1; ++i) output[i] = '*';
 
 // Copy the last character
 output[len - 1] = input[len - 1];
 output[len] = '\0';
}

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Associate III
Oct 25, 2024 4:03 PM UTC

Good morning GaetanGodart, the keyboard I'm using is the example of stm in which you see as you press the keys you see above what is being entered. I managed to get inside once entered all the message that is loaded in a GUI text that shows the hidden characters but I do not know how to prevent the same keyboard while pressing the hidden character is seen. I reviewed a little bit the guts of the code of the keyboard example but I could not understand well where is the variable that uses the keyboard to show what is being entered.

I hope I have been clear but if not please ask me.

In my code I implemented the keyboard as in the video of controllerstech where it adds two buttons, ok to pass from the keyboard to the text of the gui what is entered and another exit to hide the keyboard.

 

Associate III
Nov 11, 2024 12:45 PM UTC

thank you very much @GaetanGodart ,

With this I was able to move forward little by little to achieve my goal. again thanks for the follow up.

 

@Marc_LM thanks also.

GaetanGodart
ST Employee
Nov 5, 2024 9:36 AM UTC

Hello @Maximiliano and @Marc_LM ,

 

Indeed, it is not possible to change font for a single textArea at runtime.

 

Maximiliano, you can use the touchgfx_printf() method to print the value of the key in a console when running the simulator.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Senior
Mar 11, 2025 10:18 PM UTC

@Maximilianodid you find a way to have passwords in text boxes?

I am about to test a method of deriving a TextAreaWithWildcardBase like the flexButton with the "*style" composed templated classes.

Associate III
Mar 13, 2025 3:47 AM UTC

Hi @Marc_LM sorry for the delay.

Yes,I was able to solve it.

I don't remember well now but I made two buffers where one typed ****** and the other the password. then I added a button which if pressed showed one buffer or the other in the text on the screen.

What I had to take into account is that in the keyboard function if I pressed any key that was not a character (e.g. shift or upper case) it failed and I could not type another character, so I used the following to check before if it was a character or not by giving an ascii code range.

 

void CustomKeyboard::keyPressedhandler(Unicode::UnicodeChar keyChar)
{


	if(modo_password == 1 && keyChar >= 0x20 && keyChar <= 0x7E)
	{
		ContrasenaBuffer2[pos_pswrd]=keyChar;
		pos_pswrd++;
		// Replace the actual key character with '*'
		keyChar = '*';
		//touchgfx_printf(keyChar);

		// Add the '*' character to the buffer
		uint16_t pos = keyboard.getBufferPosition()-1;
		if (pos < BUFFER_SIZE - 1)
		{
			buffer[pos] = keyChar;
			keyboard.setBufferPosition(pos + 1);
		}
	}
	else{

	}

}

I hope I can help you.

 

 

Senior
Mar 13, 2025 1:52 PM UTC

Thanks for the confirmation.
I did tried exploring overloading the "TextAreaWithWildcardBase::draw" to hide the wildcards but that function is not virtual.

I finished testing my implementation yesterday with double buffers.
I guess Gaetan's suggestion was the most reasonable compromise.