Skip to main content
Associate III
April 20, 2024
Solved

TextArea doesnt show any text

  • April 20, 2024
  • 1 reply
  • 1772 views

I tried to show text via textArea, i put some string into translation field, i see the string in designer but when i ran it the text is not present. I tried similar thing with digital clock with same result. I tried define own typographies with or without wildccards and non generated texts but all with the same result. I tried it on real hardware, other things like images and buttons are visible but the text in textArea not. Should i call some method for rest of init textArea?

Best answer by Petr3

Now it works! I unchecked Binary font files box in Config -> Text Configuration and all texts are visible in simulator and hardware.

1 reply

mƎALLEm
ST Technical Moderator
April 20, 2024

Hello,

Did you call:

textArea.invalidate();

 after setting the string?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Petr3Author
Associate III
April 20, 2024

No, i put initial value in the TouchGFX Designer only. I didn't change the string by my custom firmware yet. I can try call that in the method screenView::setupScreen()

MM..1
Chief III
April 20, 2024

TouchGFX version?