2022-05-05 6:04 AM
I use CubeIDE 1.9.0
MCU packate STM32H7 V1.10.0
My project generates separate files for each hardware. In this case "dcmi.c" and "dcmi.h"
DCMI is set to Slave 10 bits External Synchro
I use DCMI_PSSI DMA1 Stream 2 Perpheral to Memory
CubeIDE generates following lines in HAL_DCMI_MspInit
__HAL_LINKDMA(dcmiHandle,hdmarx,hdma_dcmi_pssi);
__HAL_LINKDMA(dcmiHandle,hdmatx,hdma_dcmi_pssi);
Both of these lines fail with
../Core/Src/dcmi.c:161:5: note: in expansion of macro '__HAL_LINKDMA'
161 | __HAL_LINKDMA(dcmiHandle,hdmarx,hdma_dcmi_pssi);
| ^~~~~~~~~~~~~
../Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_hal_def.h:65:43: error: 'DCMI_HandleTypeDef' {aka 'struct __DCMI_HandleTypeDef'} has no member named 'hdmatx'
65 | (__HANDLE__)->__PPP_DMA_FIELD__ = &(__DMA_HANDLE__); \What is the correct way of handling this?
For now, I just comment these lines out. DMA seems to work...
dcmi.c
/* Several peripheral DMA handle pointers point to the same DMA handle.
Be aware that there is only one channel to perform all the requested DMAs. */
__HAL_LINKDMA(dcmiHandle,DMA_Handle,hdma_dcmi_pssi);
//__HAL_LINKDMA(dcmiHandle,hdmarx,hdma_dcmi_pssi);
//__HAL_LINKDMA(dcmiHandle,hdmatx,hdma_dcmi_pssi);Is this a bug in FW-Package?
Is "commenting out" the correct workaround?
Thanks for your help
Johannes
Solved! Go to Solution.
2022-11-28 6:36 AM
Hello @Johannes ,
This issue is fixed in STM32CubeMX latest release.
V6.7.0 is now available under this Link.
Thanks for your contribution :smiling_face_with_smiling_eyes:
Sara.
2022-05-09 9:13 AM
Hi @Johannes ,
That looks like an issue with STM32CubeMX generated code.
@Sara BEN HADJ YAHYA do you confirm it?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-05-10 4:20 AM
Hello @Johannes ,
Thanks for your feedback,
These three lines are generated whereas the Request is for DCMI IP or for PSSI IP . A specific comment is added to inform that only one LINK will be useful.
* Several peripheral DMA handle pointers point to the same DMA handle.
Be aware that there is only one channel to perform all the requested DMAs. */
__HAL_LINKDMA(hpssi,DMA_Handle,hdma_dcmi_pssi);
__HAL_LINKDMA(hpssi,hdmarx,hdma_dcmi_pssi);
__HAL_LINKDMA(hpssi,hdmatx,hdma_dcmi_pssi);The needed request should be kept and the others should be commented as you did. Please make sure to comment the unneeded lines each time you re-generate the code.
I submitted a ticket to the dev team to see if they can change the code generation and keep only the needed DMA request. I will keep you posted.
Internal ticket number: 128188 (This is an internal tracking number and is not accessible or usable by customers).
If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)
Sara.
2022-11-28 6:36 AM
Hello @Johannes ,
This issue is fixed in STM32CubeMX latest release.
V6.7.0 is now available under this Link.
Thanks for your contribution :smiling_face_with_smiling_eyes:
Sara.
2023-07-13 7:57 AM
Hello,
I am using V6.9.0. However, still encountering problem that occurs during initialization from CUBEMX. Following lines are generate the error.
/* DCMI DMA DeInit */
HAL_DMA_DeInit(hdcmi->DMA_Handle);
HAL_DMA_DeInit(hdcmi->hdmarx);
HAL_DMA_DeInit(hdcmi->hdmatx);
Error code is:
../Core/Src/stm32h7xx_hal_msp.c: In function 'HAL_DCMI_MspDeInit':
../Core/Src/stm32h7xx_hal_msp.c:226:25: error: 'DCMI_HandleTypeDef' has no member named 'hdmarx'
226 | HAL_DMA_DeInit(hdcmi->hdmarx);
| ^~
../Core/Src/stm32h7xx_hal_msp.c:227:25: error: 'DCMI_HandleTypeDef' has no member named 'hdmatx'
227 | HAL_DMA_DeInit(hdcmi->hdmatx);
| ^~
After commenting lines that generate the error, DCMI is somehow works but other code blocks are not working. I there another solution beyond updating CubeMx or commenting those lines?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.