cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F433: How to blink individual segments in the LCD?

Ten1
Associate

I can't figure this out, I know how to set the different blink modes:

LCD_BLINKMODE_SEG0_COM0, (Blink enabled on SEG[0], COM[0] (1 pixel))

LCD_BLINKMODE_SEG0_ALLCOM (Blink enabled on SEG[0], all COM (up to 8 pixels))

LCD_BLINKMODE_ALLSEG_ALLCOM   (Blink enabled on all SEG and all COM (all pixels))

...and this works, but it should be possible to select which segments should blink with ALLSEG ALLCOM selected, right? How can I do that, or is it not possible?

A second question (possible related to the question above), what is the purpose of RAMRegisterMask (specifies the LCD RAM Register Data Mask)?

I get the same result on the LCD whether I set the mask to all 1s or all 0s in HAL_LCD_Write calls, there must be some thing I'm missing?

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0