Skip to main content
Qqixi.1
Associate II
May 18, 2020
Question

Stemwin transplant for stm32f103 MCU fail.if i include "GUI.h" in main.c the problem income.

  • May 18, 2020
  • 5 replies
  • 1581 views

Error message

*** Using Compiler 'V5.06 update 4 (build 422)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'

Build target 'QD-TFT'

compiling main.c...

..\STemWin544\inc\GUI_Type.h(64): error: #20: identifier "LCD_COLOR" is undefined

 typedef LCD_COLOR    GUI_COLOR;

..\STemWin544\inc\GUI_Type.h(65): error: #20: identifier "LCD_LOGPALETTE" is undefined

 typedef LCD_LOGPALETTE GUI_LOGPALETTE;

..\STemWin544\inc\GUI_Type.h(66): error: #20: identifier "LCD_DRAWMODE" is undefined

 typedef LCD_DRAWMODE  GUI_DRAWMODE;

..\STemWin544\inc\GUI_Type.h(67): error: #20: identifier "LCD_RECT" is undefined

 typedef LCD_RECT    GUI_RECT;

..\STemWin544\inc\GUI_Type.h(74): error: #20: identifier "U8" is undefined

              const U8 * pPixel, 

..\STemWin544\inc\GUI_Type.h(75): error: #20: identifier "LCD_LOGPALETTE" is undefined

              const LCD_LOGPALETTE * pLogPal, 

..\STemWin544\inc\GUI_Type.h(78): error: #20: identifier "U32" is undefined

  GUI_COLOR (* pfIndex2Color)(

CD_PIXELINDEX Index);

..\STemWin544\inc\GUI_Type.h(83): error: #20: identifier "U8" is undefined

              const U8 * pPixel, 

..\STemWin544\inc\GUI_Type.h(84): error: #20: identifier "LCD_LOGPALETTE" is undefined

              const LCD_LOGPALETTE * pLogPal, 

..\STemWin544\inc\GUI_Type.h(87): error: #20: identifier "LCD_API_COLOR_CONV" is undefined

  const LCD_API_COLOR_CONV * pColorConvAPI;

..\STemWin544\inc\GUI_Type.h(91): error: #20: identifier "U16P" is undefined

  U16P XSize;

..\STemWin544\inc\GUI_Type.h(92): error: #20: identifier "U16P" is undefined

  U16P YSize;

..\STemWin544\inc\GUI_Type.h(93): error: #20: identifier "U16P" is undefined

  U16P BytesPerLine;

..\STemWin544\inc\GUI_Type.h(94): error: #20: identifier "U16P" is undefined

  U16P BitsPerPixel;

..\STemWin544\inc\GUI_Type.h(95): error: #20: identifier "U8" is undefined

  const U8 * pData;

..\STemWin544\inc\GUI_Type.h(106): error: #20: identifier "U16" is undefined

  U16 ID;

..\STemWin544\inc\GUI_Type.h(107): error: #20: identifier "U16" is undefined

  U16 Format;

..\STemWin544\inc\GUI_Type.h(108): error: #20: identifier "U16" is undefined

  U16 XSize;

..\STemWin544\inc\GUI_Type.h(109): error: #20: identifier "U16" is undefined

  U16 YSize;

..\STemWin544\inc\GUI_Type.h(110): error: #20: identifier "U16" is undefined

  U16 BytesPerLine;

..\STemWin544\inc\GUI_Type.h(111): error: #20: identifier "U16" is undefined

  U16 BitsPerPixel;

..\STemWin544\inc\GUI_Type.h(112): error: #20: identifier "U16" is undefined

  U16 NumColors;

..\STemWin544\inc\GUI_Type.h(113): error: #20: identifier "U16" is undefined

  U16 HasTrans;

..\STemWin544\inc\GUI_Type.h(118): error: #20: identifier "U32" is undefined

  U32  v;

..\STemWin544\inc\GUI_Type.h(134): error: #20: identifier "U8" is undefined

  U8 Pressed;

..\STemWin544\inc\GUI_Type.h(135): error: #20: identifier "U8" is undefined

  U8 Layer;

..\STemWin544\inc\GUI_Type.h(185): error: #20: identifier "I16P" is undefined

  I16P c0;

..\STemWin544\inc\GUI_Type.h(186): error: #20: identifier "I16P" is undefined

  I16P c1;

..\STemWin544\inc\GUI_Type.h(190): error: #20: identifier "U16P" is undefined

  U16P FirstChar;

..\STemWin544\inc\GUI_Type.h(191): error: #20: identifier "U16P" is undefined

  U16P LastChar;

..\USER\main.c: 0 warnings, 30 errors

"..\OBJ\TOUCH.axf" - 30 Error(s), 0 Warning(s).

Target not created.

Build Time Elapsed: 00:00:01

I do not this problem why income.

This topic has been closed for replies.

5 replies

TDK
May 18, 2020

Looks like you need to #include "LCD.h".

"If you feel a post has answered your question, please click ""Accept as Solution""."
Qqixi.1
Qqixi.1Author
Associate II
May 18, 2020

include in whats file?main.c already include this" LCD.h"​ but is not used,

Qqixi.1
Qqixi.1Author
Associate II
May 18, 2020

this is message

TDK
May 18, 2020

Well the compiler isn't finding them. Make sure it's included before whatever include file needs it. Trace your include files to ensure it can see the definitions it's complaining about. The order of includes matters.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Qqixi.1
Qqixi.1Author
Associate II
May 18, 2020
  • I used others transplant project compiler is not problem,but transplant my project alreadly problem.I'm going over it.
  • thanks you!