Skip to main content
Associate III
September 18, 2024
Solved

Standard SPI memory without FMC and Touch GFX

  • September 18, 2024
  • 1 reply
  • 707 views

Hello,

i have question about external memory storage.

Can be external serial memory used as a storage for Touch GFX images connected via standard SPI(MISO,MOSI, SCK and software driven NCS) to the MCU STM32F767 without FMC_NCS? Is it possible?

 

Thanks

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

I don't think so. Memory needed by TouchGFX needs to be in memory mapped mode. Memories using SPI interface (MOSI/MISO) don't offer this possibility. Only xSPI memories (SPI flavor) can do that. Or external memories using FMC interface.

Or may be you need to copy your images from your SPI in an internal RAM, than let TouchGFX fetches the images from that address. I'm not expert of TouchGFX but I think it could be doable but not efficient in term of application performance.

Hope I answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 18, 2024

Hello,

I don't think so. Memory needed by TouchGFX needs to be in memory mapped mode. Memories using SPI interface (MOSI/MISO) don't offer this possibility. Only xSPI memories (SPI flavor) can do that. Or external memories using FMC interface.

Or may be you need to copy your images from your SPI in an internal RAM, than let TouchGFX fetches the images from that address. I'm not expert of TouchGFX but I think it could be doable but not efficient in term of application performance.

Hope I answered your question.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.