Skip to main content
Associate
Aug 1, 2023 1:29 PM UTC
Solved

Re: STM32F769I-DISCO - Really noisy TFT LCD display

Hi everyone

i worked fine with MB116-A03 display and now i have the same problem with A09 display. I made the changes available on github:
- created the new component nt35510 with the three files (.h .c .html)
- and made changes to 4 files: stm32f769i_discovery_lcd (.c and .h) stm32f769i_discovery (.c and .h).

However the display still does not work. But are there other changes to be made? It says to enable the correct hardware target, but where can I do that?
In the stm32f769i_discovery.h file I have already reported the lines:
#if !defined(USE_STM32F769I_DISCO) && \
!defined(USE_STM32F769I_DISCO_REVB03)
#define USE_STM32F769I_DISCO

Thanks to anyone who can give me directions.

    This topic has been closed for replies.
    KDJEM.1
    KDJEM.1Best answer
    ST Technical Moderator
    Aug 1, 2023 2:22 PM UTC

    Hello @MikParà and welcome to community :),

    Please download and use the correct drivers file shared in the GitHub in your project.

    Also when  STM32F769I DISCOVERY w/ MB1166-A09 LCD daughter board connected on it should be used in stm32f769i_discovery.h file

    #define USE_STM32F769I_DISCO_REVB03

    instead

    #define USE_STM32F769I_DISCO

    Please let me know if the issue is solved.

    Thank you.

    Kaouthar

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

    2 replies

    KDJEM.1
    KDJEM.1Best answer
    ST Technical Moderator
    Aug 1, 2023 2:22 PM UTC

    Hello @MikParà and welcome to community :),

    Please download and use the correct drivers file shared in the GitHub in your project.

    Also when  STM32F769I DISCOVERY w/ MB1166-A09 LCD daughter board connected on it should be used in stm32f769i_discovery.h file

    #define USE_STM32F769I_DISCO_REVB03

    instead

    #define USE_STM32F769I_DISCO

    Please let me know if the issue is solved.

    Thank you.

    Kaouthar

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
    MikParàAuthor
    Associate
    Aug 4, 2023 10:25 AM UTC

    Good morning everyone
    thanks for the advice, I solved it and it started working again
    Thanks again for your support