New STM32H747-DISCO example problems.
Hi There,
I have a new STM32H747-DISCO here.
The board came without the demo flashed on it, also the demo can not be flashed, see here: https://community.st.com/s/question/0D53W00002ASl3lSAD/stm32h747-discovery-blank
Most of the examples in the cube package concerning the lcd do not work, see here: https://community.st.com/s/question/0D53W00002A3uJaSAJ/stm32h747-lcd-display-issue
The BSP example doesn't build, the project import looks wonky, links are incorrect.
Some stemwin examples that build will not flash, for example STemWin_acceleration_CM7.
As the linked problems have also been posted very recently is there a new revision of this board that is not compatible with the examples?
I have tried STMCubeIde 1.11 and 1.12, also tried on windows, linux and even a Mac.
Exact same issues on all of them.
Anyone any ideas how to progress here as basically very little is working!