Skip to main content
JLee.32
Associate III
May 13, 2021
Question

How to shorten the programming flash time for a project with TouchGFX?

  • May 13, 2021
  • 0 replies
  • 447 views

Due to lots of image files for UI, I need to spend around 3~4 minutes programming the external flash. Can I specify a code area and an image area for the extenal flash? Then if image files are not changed, can I just update the code area?

Or is there any way to shorten the programming flash time for a project with TouchGFX?

This topic has been closed for replies.