Hello @YCF.1 ,
A good starting point is to analyze the ListLayout example in TouchGFXDesigner.
You will see in MainView.cpp that a callback "listElementClicked" is implemented. This method will be called every time the user clicks on the button "Delete" and provides the specific CustomListElement object that was clicked. That's already a good way to isolate each element of your list.
Then, if you want to get the specific index of the clicked element of your list, you can try that :
- Declare an integer variable in CustomListElement.hpp, like this :
int itemIndex;
- Modify the setupListElement(const Bitmap&,TEXTS) method to include that new parameter.
void setupListElement(const Bitmap& iconBMP, TEXTS iconTextID, int elementIndex);
- In CustomListElement.cpp, also modify the setupListElement(const Bitmap&,TEXTS) method to allow the user to store the items indexes in this class.
void CustomListElement::setupListElement(const Bitmap& iconBMP, TEXTS iconTextID, int elementIndex)
{
itemIndex = elementIndex;
icon.setBitmap(iconBMP);
text.setTypedText(TypedText(iconTextID));
text.resizeToCurrentText();
invalidate();
}
- Then, in MainView.cpp, fix the call of this function in the setupScreen() method. For instance, there is the function to define the Bitmap and text displayed on the first element. I just defined the element index at "0" here.
listElements[0].setupListElement(Bitmap(BITMAP_ICON0_ID) , T_LIST_ELEMENT_00 , 0);
- Finally, in the listElementClicked(CustomListElement&) function, you can get the selected item number like this :
int item_nr = element.itemIndex; // "element" is a CustomListElement here
I will also join my project to this post, it might be easier for your understanding.
Let me know if that helped or if you have other questions,
/Yoann