Skip to main content
Associate II
February 8, 2024
Solved

How to edit Dynamic Graph in TouchGFX to print time in X-Axis ?

Hello everyone, I hope you are all having a great day. I would like to know how to work with the labels for the dynamic graph widget :

purushotham2608_0-1707376315812.png

 

I want to know how to make the X axis labels display a real time value instead of numbers and I want it to be accurate to the real time, for example : Instead of 10,20  etc I want it to show 01:10 AM, 01:20 AM. etc. can someone help me with this please? Thank You Best Regards.

 

This topic has been closed for replies.
JTP1Best answer
Graduate II
February 8, 2024

Hi

I think you cannot get time to the X labels directly from TGFX Designer:slightly_frowning_face:

You need to litte bit manipulate the GraphLabels.cpp (and maybe be GraphLabels.hpp, depends on what you want).

Browse first to \Middlewares\ST\touchgfx\framework\source\touchgfx\widgets\graph\ folder and copy GraphLabels.cpp to your project \TouchGFX\gui\src\common\ folder for example.Edit that copy in \common\ folder.

Here is simple example which prints hh:mm AM/PM format time when number of decimals is set to value 4 in TGFX designer for X Labels.

GraphLabels.cpp:

 

void GraphLabelsBase::formatLabel(Unicode::UnicodeChar* buffer, int16_t bufferSize, int label, int decimals, Unicode::UnicodeChar decimalPoint, int scale) const
{
 int length = 0;
 int scaledLabel;

 if (label < 0 && length < bufferSize - 1)
 {
 buffer[length++] = '-';
 label = -label;
 }

 if (decimals == 0)
 {
 	scaledLabel=(label + scale / 2) / scale;
 	Unicode::snprintf(buffer + length, bufferSize - length, "%d", (label + scale / 2) / scale);
 }
	/* HERE Simply Extension to print X label time */
 else if (decimals == 4) // custom print time hh:mm AM when set 4 decimal in the TGFX designer
 {
 	scaledLabel=label;
		
		// cut down the overflow (24 hours * 60 minutes)
		scaledLabel%=(24*60);

		if(scaledLabel<(12*60))
			Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d AM", scaledLabel/60,scaledLabel%60);
		else
			Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d PM", scaledLabel/60,scaledLabel%60);
 }
 else if (decimals > 0)
 {
 Unicode::snprintf(buffer + length, bufferSize - length, "%d", label / scale);
 length = Unicode::strlen(buffer);
 if (length < bufferSize - 1)
 {
 buffer[length++] = decimalPoint;
 int remainder = label % scale;
 for (int i = 0; i < decimals && length < bufferSize - 1; i++)
 {
 remainder *= 10;
 if (i == decimals - 1 || length == bufferSize - 1)
 {
 remainder += scale / 2; // Rounding on the last (visible) digit
 }
 const int digit = (remainder / scale);
 buffer[length++] = (Unicode::UnicodeChar)('0' + digit);
 remainder %= scale;
 }
 buffer[length] = (Unicode::UnicodeChar)0;
 }
 }
}

 

 

 

Note that if you do like this, one point must represent value of one minute in your data to get time domain correct !

Then, your data will naturally start from time 00:00

JTP1_3-1707412285094.png

Which is not allways the case. One way might be to add offset for starting time. So browse to \Middlewares\ST\touchgfx\framework\include\touchgfx\widgets\graph\- folder and open GraphLabels.hpp.

Add variable labelOffset and funtion 'setXStartOffset' to the X labels class.

GraphLabels.hpp:

 

class GraphLabelsX : public GraphLabelsBase
{
public:

	/** EXTENSION:
	 * Variable for X -label offset , when using extended time- type X labels
	 *
	 */
	int labelOffset=0;
	
	/** EXTENSION:
	 * Function for set X -label offset 
	 *	
	 * offset The X label offset of first the label value 
	 */
 virtual void setXStartOffset(int offset)
 {
 	labelOffset=offset;
 }

 virtual void invalidateGraphPointAt(int16_t index);

 

 

 

 Then open GraphLabels.cpp and locate GraphLabelsX::drawString- funtion. Add summing of labelOffset to the call of formatLabel. (Note that same format routine is called for X and Y labels, so this offset must be take into account here in the call).

GraphLabels.cpp:

 

void GraphLabelsX::drawString(const Rect& invalidatedArea, const Font* fontToDraw, const AbstractDataGraph* graph, const int valueScaled, const int labelScaled, const uint8_t a) const
{
 const int16_t labelX = valueToScreenXQ5(graph, valueScaled).round() - graph->getGraphAreaPaddingLeft();
 if (labelX < 0 || labelX >= graph->getGraphAreaWidth())
 {
 return;
 }

 Unicode::UnicodeChar wildcard[20];
	/*** Extension HERE - labelOffset summed with label- value: */
 formatLabel(wildcard, 20, labelOffset+getIndexToXAxis(graph, valueScaled, labelScaled), labelDecimals, labelDecimalPoint, graph->getScaleX());
 // Adjust to make label centered
 int16_t labelWidth;
 const Unicode::UnicodeChar* text = labelTypedText.getText();

 

 

 

 Then you can set in your view.cpp something like

 

 

 

dynamicGraph1MajorXAxisLabel.setXStartOffset((11*60)+45); //11:45 AM

 

 

 

And then time starts from 11:45 AM

JTP1_2-1707412217725.png

Here are the most important settings of graph in this example:

JTP1_4-1707412695956.png

Number of decimals is set to 4 to activate extended time formatting for X labels. Since the Y label uses the same formatLabel function, there is must something that activates Time format for x labels but not for y (in most cases not needed to have time also in Y label).

This is just simple example how to extend DynamicGraph.

Hope this helps somebody.

Br JTP

2 replies

JTP1Best answer
Graduate II
February 8, 2024

Hi

I think you cannot get time to the X labels directly from TGFX Designer:slightly_frowning_face:

You need to litte bit manipulate the GraphLabels.cpp (and maybe be GraphLabels.hpp, depends on what you want).

Browse first to \Middlewares\ST\touchgfx\framework\source\touchgfx\widgets\graph\ folder and copy GraphLabels.cpp to your project \TouchGFX\gui\src\common\ folder for example.Edit that copy in \common\ folder.

Here is simple example which prints hh:mm AM/PM format time when number of decimals is set to value 4 in TGFX designer for X Labels.

GraphLabels.cpp:

 

void GraphLabelsBase::formatLabel(Unicode::UnicodeChar* buffer, int16_t bufferSize, int label, int decimals, Unicode::UnicodeChar decimalPoint, int scale) const
{
 int length = 0;
 int scaledLabel;

 if (label < 0 && length < bufferSize - 1)
 {
 buffer[length++] = '-';
 label = -label;
 }

 if (decimals == 0)
 {
 	scaledLabel=(label + scale / 2) / scale;
 	Unicode::snprintf(buffer + length, bufferSize - length, "%d", (label + scale / 2) / scale);
 }
	/* HERE Simply Extension to print X label time */
 else if (decimals == 4) // custom print time hh:mm AM when set 4 decimal in the TGFX designer
 {
 	scaledLabel=label;
		
		// cut down the overflow (24 hours * 60 minutes)
		scaledLabel%=(24*60);

		if(scaledLabel<(12*60))
			Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d AM", scaledLabel/60,scaledLabel%60);
		else
			Unicode::snprintf(buffer + length, bufferSize - length, "%02d:%02d PM", scaledLabel/60,scaledLabel%60);
 }
 else if (decimals > 0)
 {
 Unicode::snprintf(buffer + length, bufferSize - length, "%d", label / scale);
 length = Unicode::strlen(buffer);
 if (length < bufferSize - 1)
 {
 buffer[length++] = decimalPoint;
 int remainder = label % scale;
 for (int i = 0; i < decimals && length < bufferSize - 1; i++)
 {
 remainder *= 10;
 if (i == decimals - 1 || length == bufferSize - 1)
 {
 remainder += scale / 2; // Rounding on the last (visible) digit
 }
 const int digit = (remainder / scale);
 buffer[length++] = (Unicode::UnicodeChar)('0' + digit);
 remainder %= scale;
 }
 buffer[length] = (Unicode::UnicodeChar)0;
 }
 }
}

 

 

 

Note that if you do like this, one point must represent value of one minute in your data to get time domain correct !

Then, your data will naturally start from time 00:00

JTP1_3-1707412285094.png

Which is not allways the case. One way might be to add offset for starting time. So browse to \Middlewares\ST\touchgfx\framework\include\touchgfx\widgets\graph\- folder and open GraphLabels.hpp.

Add variable labelOffset and funtion 'setXStartOffset' to the X labels class.

GraphLabels.hpp:

 

class GraphLabelsX : public GraphLabelsBase
{
public:

	/** EXTENSION:
	 * Variable for X -label offset , when using extended time- type X labels
	 *
	 */
	int labelOffset=0;
	
	/** EXTENSION:
	 * Function for set X -label offset 
	 *	
	 * offset The X label offset of first the label value 
	 */
 virtual void setXStartOffset(int offset)
 {
 	labelOffset=offset;
 }

 virtual void invalidateGraphPointAt(int16_t index);

 

 

 

 Then open GraphLabels.cpp and locate GraphLabelsX::drawString- funtion. Add summing of labelOffset to the call of formatLabel. (Note that same format routine is called for X and Y labels, so this offset must be take into account here in the call).

GraphLabels.cpp:

 

void GraphLabelsX::drawString(const Rect& invalidatedArea, const Font* fontToDraw, const AbstractDataGraph* graph, const int valueScaled, const int labelScaled, const uint8_t a) const
{
 const int16_t labelX = valueToScreenXQ5(graph, valueScaled).round() - graph->getGraphAreaPaddingLeft();
 if (labelX < 0 || labelX >= graph->getGraphAreaWidth())
 {
 return;
 }

 Unicode::UnicodeChar wildcard[20];
	/*** Extension HERE - labelOffset summed with label- value: */
 formatLabel(wildcard, 20, labelOffset+getIndexToXAxis(graph, valueScaled, labelScaled), labelDecimals, labelDecimalPoint, graph->getScaleX());
 // Adjust to make label centered
 int16_t labelWidth;
 const Unicode::UnicodeChar* text = labelTypedText.getText();

 

 

 

 Then you can set in your view.cpp something like

 

 

 

dynamicGraph1MajorXAxisLabel.setXStartOffset((11*60)+45); //11:45 AM

 

 

 

And then time starts from 11:45 AM

JTP1_2-1707412217725.png

Here are the most important settings of graph in this example:

JTP1_4-1707412695956.png

Number of decimals is set to 4 to activate extended time formatting for X labels. Since the Y label uses the same formatLabel function, there is must something that activates Time format for x labels but not for y (in most cases not needed to have time also in Y label).

This is just simple example how to extend DynamicGraph.

Hope this helps somebody.

Br JTP

ST Employee
February 29, 2024

Hello all,


Just don't forget to add wildcard characters to your topography with JTP1's solution :

Regards,

Louis BOUDOST Software Engineer | TouchGFX