Skip to main content
gregstm
Senior II
March 2, 2020
Question

Generating VGA pixel clock hint (640x480@60Hz=>25.175MHz pixel clock)

  • March 2, 2020
  • 3 replies
  • 4092 views

I decided to have a go at producing a VGA display with the STM32L4. 

640x480 @ 60Hz is the lowest resolution compatible with most displays (and VGA to HDMI convertors - many TVs only have HDMI ports these days). This resolution requires a pixel clock of 25.175MHz, which is usually derived from a crystal.

But you can get close to this frequency using the PLL. Set the MSI to 24MHz, the input divider to 5 (/M) and the multiplier to 21 - this produces a VCO frequency of 100.8MHz, which divides down to 50.4MHz (for the System clock) and 25.2MHz (for SPI/Pixel clock).

25.2MHz is only 0.1% off from 25.175, which should work (haven't quite finished off the rest of the software yet.....).

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
March 2, 2020

A few random remarks:

  • I'm not sure I would use an RC oscillator to generate video timing.
  • provided the signal is going to be fed to a known destination which is OK with the RC oscillator jitter/drift, it might be quite well be OK with a frequency mismatch, too
  • some RC oscillators in STM32s can be fine-tuned/trimmed (although usually the step is relatively coarse)
  • it might be fun to find a 25.175MHz crystal :)

JW

Nikita91
Lead II
April 16, 2020

This article might interest you. It seems difficult to get stable timing but it is possible.

http://cliffle.com/blog/pushing-pixels/

gregstm
gregstmAuthor
Senior II
April 22, 2020

Thanks for the article Nikita91. I did try my method of generating a 25.2Mhz using the MSI and found that it didn't look too bad on a small monitor, but when I put it up on a large TV it was very wobbly - it turned out to be a great way of visualising clock jitter (..the expression "don't count your chickens before they hatch" comes to mind).

My original aim for using 640x480 @60Hz was to minimise RAM and processor usage on a STM32L chip. Thankfully the 640x480 @ 72Hz (31.5MHz pixel clock) is just as easy to produce - but you need to use a 4MHz (or 8MHz/16MHz) crystal (4MHz x 63=> 252MHz, /4=>63MHz, /2=>31.5MHz). This resulted in a rock solid display - but I still need to fine tune the Hblank/Vblank timings (when I get the time to revisit it). To ensure unvarying timing and minimise interrupt overhead, I DMA the whole screen in one block (rather than using a line by line DMA) - it does mean you lose some extra memory for the horizontal blanked areas.