Skip to main content
Associate II
January 31, 2024
Question

TouchGFX firmware has a dependency on STM32CubeProgrammer

  • January 31, 2024
  • 5 replies
  • 1771 views

Hi,

As the title says the firmware I'm working on, which has been created using TouchGFX, will not work without having STM32CubeProgrammer installed on the system. Does anyone have any ideas as to why this could be or any drivers etc. that I could maybe use as a dependency instead?
Many thanks

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
January 31, 2024

@remodivito wrote:

will not work without having STM32CubeProgrammer installed on the system. 


Please explain what you mean by that:

  • The code won't build on your host machine?
  • You can't load the code onto your target?
  • The code doesn't run on the target?
  • other?
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
January 31, 2024

The program is for updating the firmware. It fails to recognise the ST-Link hardware without CubeProgrammer installed

 

 

Tesla DeLorean
Guru
January 31, 2024

Perhaps state what board you're using, and which USB connector on that board.

Sounds like it is looking for a driver that STM32 Cube Programmer installs, you could install that driver independently.

Why are you connecting it to a computer? Does it need USB for some other purpose, or just to power the board? If just powering, consider a Charging Only cable, without the data wires.

Depending on board, check for jumpers related to powering options.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
February 1, 2024

Find the whole driver archive under the STM32 Cube Programmer Install directories.  STM32CubeProgrammer_v2.15.0\Drivers\DFU_Driver\Driver\SignedDrivers ...

Went here  https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32-device-cannot-be-recognised-without-stm32cubeprogrammer/td-p/634688

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..