Skip to main content
BGasy.1
Associate II
July 12, 2022
Question

Wrong CRC-32 — HAL_CRC_Calculate output on STM32F401CCU6 Blackpill

  • July 12, 2022
  • 5 replies
  • 10822 views

I've been implementing I2C communication between F401CCU6 and Nucleo F746ZG, while adding CRC I got different outputs, Nucleo provides configurable CRC peripheral, while F401 is by default set to 0x4C11DB7 (https://www.st.com/resource/en/reference_manual/rm0368-stm32f401xbc-and-stm32f401xde-advanced-armbased-32bit-mcus-stmicroelectronics.pdf#page=68&zoom=100,89,116)0693W00000QKxkCQAT.pngIt also provides reseting initial value to 0xFFFF FFFF, ("The CRC calculator can be reset to 0xFFFF FFFF with the RESET control bit in the CRC_CR register. This operation does not affect the contents of the CRC_IDR register")

I've set Nucleo CRC polynomial, init value to match those on BlackPill. Calculated value matches with CRC-32/MPEG-2 standard (available at https://crccalc.com/ for example).

Did anyone has experienced this too?

This topic has been closed for replies.

5 replies

waclawek.jan
Super User
July 12, 2022

Details matter.

Observe/compare exactly how do you (and any "library" you've used is now your program and your responsibility) set up and feed the CRC register in both cases. Observe/compare during execution - perhaps single-stepping in disasm, to see exactly how data are fed - how the CRC registers content changes, as being fed.

> Calculated value matches with CRC-32/MPEG-2 standard

In the 'F7 or in the 'F4? As they don't match each other, only one of them may match any "standard".

Probably, data need to be fed byte-wise to achieve this. Or, in words they have to be swapped, as the CRC peripheral is big endian (MSByte-first), unlike the common expectation.

JW

BGasy.1
BGasy.1Author
Associate II
July 12, 2022

I've been testing it that way:

uint8_t test_crc[] = "12345";
uint32_t crc_val = HAL_CRC_Calculate(&hcrc, (uint32_t*)test_crc, sizeof(test_crc)-1);

Nucleo spits out 0xBD9AB747 as it should be according to crccalc, the point is, if F4 polynomial is 0x4C11DB7 as stated in manual, and init value was reset to 0xFFFF FFFF accordingly, then why the result is different (0x5355ffb1)?

I've used both

__HAL_RCC_CRC_CLK_ENABLE() and MX_CRC_Init() and when fed different data it

BGasy.1
BGasy.1Author
Associate II
July 12, 2022

... and when fed different data it gives different result so i guess its working (somehow)

Tesla DeLorean
Guru
July 12, 2022

It expects to be feed 32-bit words, and a word count, doesn't it?

The STM32F4 and several others in the family have a very specific and inflexible implementation, ill suited to the endian ordering at a bit and byte level.

On-line calculators often have difficulty with awkward and specific implementations due to the sensitivity of the CRC's in general to bit level nuances.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Bob S
Super User
July 12, 2022

The HAL_CRC_Calculate() "BufferLength" parameter is NOT the number of BYTES, it is the number of "words". On the F401 the "word" size is fixed at 32bits. On the F7xx it is programmable/configurable to be 8, 16 or 32 bits.

So if you use the code posted above on the F4xx, you are feeding a buffer of 5 bytes but telling it to read 5 each 32-bit words (i.e. 20 bytes).

Tesla DeLorean
Guru
July 12, 2022

>>On the F7xx it is programmable/configurable to be 8, 16 or 32 bits.

Yes, but often a bit of a beast to wrangle. Demonstrably usable for 7, 9 and 24-bit CRC too

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
July 15, 2022

> HAL_CRC_Calculate(&hcrc, (uint32_t*)test_crc, 1);

> Should be working? 

Sure. If you followed the often poorly documented way it was intended​ to be used by Cube's authors, it "works" exactly as those Cube authors intended. Which is not necessarily the same way you want, and it also may change with changing Cube version.

Use direct register access, if you want to have control ​over how it works.

JW​