Skip to main content
Mario Luzeiro
Associate III
September 26, 2019
Question

sha1_alt.c (mbedTLS implementation) bug?

  • September 26, 2019
  • 3 replies
  • 999 views

I have a file from ST, not sure where it comes from but the header has:

sha1_alt.c for SHA1 HASH

Copyright (c) 2017, STMicroelectronics

I am getting issues with the function that call HAL_HASH_SHA1_Accumulate function.

They are no checking for size/len if it is 0.

For some reason I am getting this issue but not sure if its this file or the application issue.

Shall it checks if size is >0 ?

Do you have an updated version of this file?

This topic has been closed for replies.

3 replies

Mario Luzeiro
Associate III
September 26, 2019

I also found that this functions are not working with data length not multiple of 4. Shall it handle this not multiple cases?

Tesla DeLorean
Guru
September 26, 2019

It is documented as requiring 4-byte multiple. You're expected to either use it for large block, or wrap it with some spill buffer method to meet the requirements of the underlying hardware.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Mario Luzeiro
Associate III
September 27, 2019

I found that it misses a padding as described here:

https://tools.ietf.org/html/rfc3174#section-4

mbed crypto software implementation is adding that padding:

https://github.com/ARMmbed/mbed-crypto/blob/aa2e298bde122e695c72288098a9ab3d9ac5729a/library/sha1.c#L368

so as far as I understand, this sha1_alt.c that I have is not implementing the required padding.