Skip to main content
kartik
Associate III
April 4, 2014
Question

Would like to use the UART on the STM32F429ZIT Discovery boart

  • April 4, 2014
  • 2 replies
  • 558 views
Posted on April 04, 2014 at 03:22

I would like to use one of the UARTS on the STM32F4 to connect the MCU to a Bluetooth SMART controller. I was wondering if anyone could tell me if there is any access on the board to one of the UARTs so that i can solder wires to pull the RX/TX lines out. If so, which UART is it? I'm sure going through the schematic would tell me this, but I'm a noob to the really lowlevel embedded stuff and I've been looking at the schematic for a while and still can't figure it out. Any help would be much appreciated.

Thanks

Kartik

#discovery #uart #stm32f4
This topic has been closed for replies.

2 replies

Andrew Neil
Super User
April 4, 2014
Posted on April 04, 2014 at 20:07

Have you looked at the schematics?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
April 4, 2014
Posted on April 04, 2014 at 20:48

The manual for the STM32F429I-DISCO does enumerate a pin list, if you can't decode the schematic this list would be where to start.

As I recall USART1 PA9/PA10 are available on this board.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..