Which MCUs actually have 12 bit DACs
I'm after a low power STM32 with DAC outputs.
ST Application note AN4566 states in table 1 on the first page that there are processors in all the STM32 ranges that have a 12 bit DAC. The MCU selector also doesn't make the DAC box selectable or deselectable which again implies they are commonplace.
But when I open random datasheets for the lower cost models I find very few that actually have the 12 bit DAC, the smallest so far being an STM32F103 with 256k Flash.
Is there a list somewhere of which MCUs actually have DACs ?