Skip to main content
elil1975
Associate II
November 2, 2009
Question

Which compiler is already supporting STM32L ?

  • November 2, 2009
  • 2 replies
  • 629 views
Posted on November 02, 2009 at 05:29

Which compiler is already supporting STM32L ?

    This topic has been closed for replies.

    2 replies

    elil1975
    elil1975Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:28

    Dear Sirs,

    On my work we're considering to use STM32L MCU. But the chip has not been launched yet and I haven't found on either Keil or IAR or Cosmic or Raisonance sites that they're supporting this MCU. May be anybody has an other information ?

    Thank you in advance,

    E.L.

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:28

    What do you mean by ''support''?

    A compiler is just about converting source code to machine code - so, if the machine code is the same, any existing compiler will support it!

    If you're talking about specific debug and/or simulation features, that's a different story - but it has nothing to do with the Compiler itself!