Skip to main content
Mr_M_from_G
Senior II
December 16, 2021
Solved

Where are the schematics for NUCLEO-H743ZI2

  • December 16, 2021
  • 4 replies
  • 3373 views

Hello,

I have here two Nucleos with an H743 on it. If it is rev Y, it is the "old" 144pin Nucleo board with the break-off ST-link board on top. For this there is a schematics in appendix A of the user manual. But if it is rev V, it is NUCLEO-H743ZI2 , note the 2 at the end, with no break-off possibility and a different user manual. And this manual has no schematics included. A trouble start as I start my project. While the manual says PC9 = MCO2 is on CN8 pin4 and CN12 pin1, I see a signal only on CN8 pin4. No way to check what's going on without schematics.

Please ST folks can you provide this somewhere.

Thanks a lot

Martin

Best answer by Mike_ST

Hello,

MB1137 schematics (NUCLEO-H743ZI) with ST-Link V2 : https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip

MB1364 schematics (NUCLEO-H743ZI2) with ST-Link V3 : https://www.st.com/resource/en/schematic_pack/mb1364-h743zi-c01_schematic.pdf

These links are available at the bottom of the CAD resources page:

https://www.st.com/en/evaluation-tools/nucleo-h743zi.html#cad-resources

4 replies

Sco
ST Employee
December 16, 2021

Could you share me "which user manual you rely on?"

Mr_M_from_G
Senior II
December 16, 2021

Hi Sco,

yes, sure, here are the manuals I use:

For the "old" 144pin Nucleo I have UM1974, page footer says DocID028599 Rev 7 December 2017

For the NUCLEO-H743ZI2 I have UM2407, page footer says UM2407 Rev 2, June 2020, which I downloaded just yesterday. This is the one I desire schematics for.

I hope you can help.

Martin

Mike_ST
Mike_STBest answer
ST Technical Moderator
December 16, 2021

Hello,

MB1137 schematics (NUCLEO-H743ZI) with ST-Link V2 : https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip

MB1364 schematics (NUCLEO-H743ZI2) with ST-Link V3 : https://www.st.com/resource/en/schematic_pack/mb1364-h743zi-c01_schematic.pdf

These links are available at the bottom of the CAD resources page:

https://www.st.com/en/evaluation-tools/nucleo-h743zi.html#cad-resources

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Associate II
January 15, 2024

Hello,

I bought one Nucleo-H743ZI2 board and found the two capacitors (C71 and C72) for X2 32.768KHz are not installed. May I know if I need to install them with 5.1pF if I want to use the X2? I went through the manual "UM2407 User manual for STM32H7 Nucleo-144 boards (MB1364)". But it seems not mention the two capacitors for the LSE clock. Thank you.32.768.PNG

 

mƎALLEm
ST Technical Moderator
January 15, 2024

Hello @Jiaming  and welcome to the community.

This thread is already closed and I suggest you to open a new one.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Mr_M_from_G
Senior II
December 16, 2021

Hi Mike,

thanks for this quick and complete answer - both thumbs up

Martin