Question
uwTick not incrementing.. (HAL_Delay())
Posted on December 04, 2015 at 07:58
Hi,
I called HAL_Delay(500); but inside the function, the return value of HAL_GetTick() is zero. What can be wrong? Thanks in advance.EDIT : oops, when I set a break point at line A below, I see tickstart is always 0 even when I press F10 keys many times because it can never progress. If I remove the break point and set a breakpoint there later, I see increased tickstart value. Because I called HAL_Delay(500); inside while loop, every time I see increment, it is incremented in unit of 500 ticks. I was confused by the way debugger works.__weak void HAL_Delay(__IO uint32_t Delay){ uint32_t tickstart = 0; tickstart = HAL_GetTick(); while((HAL_GetTick() - tickstart) < Delay) <=== line A { }}Chan