Skip to main content
gokhannsahin
Associate III
October 9, 2018
Question

Using the SPI module during the receiving data via DMA

  • October 9, 2018
  • 1 reply
  • 563 views

Hi everyone,

I'm using the DMA to receive the data from external flash via DMA. Can the SPI module transmit data while receiving from external flash at the same time? Or will it block this transmitting until completing the receiving? Or can simultaneous access be provided while receiving/transmitting?

With another possibility, if I try to transmit with HAL_SPI_Transmit(...) after start the DMA in order to transmit the data? It will corrupt, or will block me this request?

By the way, the SPI module is being used as full duplex.

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    October 10, 2018

    The chips you are talking too tend to be inherently sequential in operation. Any concurrent operation should be in the datasheet.

    As you're clocking back data now data is being clocked out. For SPI Flash reads this is typically a dummy or null byte that is ignored. The datasheet for the device should be illustrative. For writes status might be returned in the back channel.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..