using strtok function leads to clearing token before i can use it
I want to design a GPS car tracker that alarms when the speed reaches a certain value and I want to first test the code with the USB to TTL module which is connected to my stm32, and simulate sim808 answers. when I send the GPS information only the first time the micro responds correctly and the second time I send the GPS information the micro doesn't respond. when I debugged the code I found out that the second time the strtok function makes token zero before getting tokens and therefore the calculated values are zero. I used strtok before for getting coordinates from sim808 string without problem I don't know what's wrong here and why it works the first time? here is the string i want to get tokens from:
AT+CGNSINF\r\r\n
+CGNSINF:1,1,20210809114956.000,36.343509,59.590779,1029.500,41.25,284.6,1,,1.0,1.3,0.8,,11,7,,,29,,\r\n
\r\n
OK\r\n
here is my main code :
#include <stm32f10x.h>
#include "usart.h"
#include <string.h>
#include <stdio.h>
#include <stdlib.h>
#include <stdint.h>
#include <math.h>
char S=0x1A;
#define Enter usart_sendchar('\n');
#define CR usart_sendchar('\r');
#define GIM usart_sendchar('"');
#define SUB usart_sendchar(S);
char get_Enter = 0;
uint8_t ch;
uint8_t ch2;
char str1[400];
char str3[400];
int g=0;
int i=0;
char flag=0;
char str_tmp[20];
char str_tmp2[20];
char* p;
char* j;
int sec=0;
// cheraghchi street start point
float a=36.345135;
float b=59.548276;
// cheraghchi street end point
float c=36.325215;
float d=59.628918;
// speed limit of cheraghchi
float w=40.00;
//calling all the functions
void Send_SMS(char *text);
void Send_KEY(char *text);
void del_All_SMS(void);
void CMGF_1(void);
void CMGF_KEY(void);
void CMGR (void);
void CGNSPWR(void);
void CGNSINF(void);
void CGNSINF_t(void);
void Send_CAUTION(char *text);
void AT(void);
void Delay (uint32_t Time);
void USART1_IRQHandler(void);
void interrupt_activation(void);
void EXTI3_IRQHandler(void);
void EXTI1_IRQHandler(void);
void EXTI2_IRQHandler(void);
void Delay (uint32_t Time)
{
uint32_t i;
i = 0;
while (Time--) {
for (i = 0; i < 5000; i++);
}
}
void timer_init(void) {
RCC->APB2ENR |= (1<<3);
GPIOB->CRL &=~0xF;
GPIOB->CRL |= 0x3; //////// GPIOB.0 output push pull
RCC->APB2ENR |= (1<<11); /* enable clock for TIM1 */
TIM1->PSC = ( 7200 - 1); /* set prescaler = 10KHz */
TIM1->ARR = ( 5000 - 1); /* set auto-reload = 500 ms */
TIM1->DIER = (1<<0); /* Update Interrupt enable */
TIM1->CR1 |= (1<<0); /* 0x0001 timer enable */
NVIC_SetPriority(TIM1_UP_IRQn,1);
}
void TIM1_UP_IRQHandler (void)
{
sec++;
if (TIM1->SR & (1<<0))
{
if (sec==10)
{
str_tmp[0]='\0';
strcpy(str_tmp,"AT+CGNSINF");
usart_sendstring(str_tmp);
Enter
CR
}
else if (sec==20)
{
if (p)
{
float e[7];
float m; //for latitude
float n; //for longitude
float z; //for speed
char str2[80];
const char s[2] = ",";
char *token;
// getting the lattitude and longitude
token = strtok(p, s);
for (int i=0;i<7;i++){
sprintf( str2," %s", token );
e[i]=atof(str2);
token = strtok(NULL, s);
}
token=NULL;
m=e[3];// latitude
n=e[4]; // longitude
z=e[6]; // speed
if (m<a && m>c && n>b && n<d) {
if (z>w)
{
Send_CAUTION("CAUTION ! illegal speed ");
sec=0; // for illegal speed
p=NULL;
for (int i=0;i<7;i++){
e[i]=0;
}
}
sec=0; // for normal speed
}
sec=0; // for out of range streets
}
}
}
TIM1->SR &= ~0x1;
}
void CMGF_CAUTION(void)
{
str_tmp[0]='\0';
strcpy(str_tmp,"AT+CMGF=1");
usart_sendstring(str_tmp);
Enter
CR
}
void Send_CAUTION(char *text)
{
CMGF_CAUTION();
str_tmp[0]='\0';
strcpy(str_tmp,"AT+CMGS=");
usart_sendstring(str_tmp);
GIM
str_tmp[0]='\0';
strcpy(str_tmp,"+98905xxx6399");
usart_sendstring(str_tmp);
GIM
Enter
CR
usart_sendstring(text);
Enter
CR
str_tmp[0]='\0';
SUB
del_All_SMS();
}
void Send_SMS(char *text)
{
CMGF_1();
Delay(500);
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"AT+CMGS=");
Delay(500);
usart_sendstring(str_tmp);
GIM
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"+98905xxx6399");
Delay(500);
usart_sendstring(str_tmp);
GIM
Enter
CR
Delay(500);
usart_sendstring(text);
Enter
CR
str_tmp[0]='\0';
Delay(500);
SUB
Delay(100);
del_All_SMS();
}
void USART1_IRQHandler(void) {
ch = USART1->DR & 0xFF;
ch2 = USART1->DR & 0xFF;
if (str1[346]!=NULL) {
for (int j=0;j<400;j++)
{
str1[j]=0;
}
i=0;
}
else if (str3[240]!=NULL)
for (int g=0;g<400;g++)
{
str3[g]=0;
}
else {
str1[i]= ch;
str3[g]=ch2;
i++;
g++;
}
}
void CGNSINF_t(void)
{
str_tmp[0]='\0';
strcpy(str_tmp,"AT+CGNSINF");
usart_sendstring(str_tmp);
Enter
CR
}
void CMGF_1(void)
{
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"AT+CMGF=1");
Delay(500);
usart_sendstring(str_tmp);
Enter
CR
}
void del_All_SMS(void)
{
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"AT+CMGD=1,4");
Delay(500);
usart_sendstring(str_tmp);
Enter
CR
}
void CMGR(void)
{
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"AT+CMGR=1");
Delay(500);
usart_sendstring(str_tmp);
Enter
CR
}
void CGNSINF(void)
{
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"AT+CGNSINF");
Delay(500);
usart_sendstring(str_tmp);
Enter
CR
}
void CGNSPWR_1(void)
{
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"AT+CGNSPWR=1");
Delay(500);
usart_sendstring(str_tmp);
Enter
CR
}
void AT(void)
{
str_tmp[0]='\0';
Delay(100);
strcpy(str_tmp,"AT");
Delay(500);
usart_sendstring(str_tmp);
Enter
CR
}
int main()
{
SystemInit();
usart_init();
timer_init();
AT();
check:AT();
Delay(2000);
p=strstr(str1,"OK");
if(p==NULL) goto check;
CMGF_1();
Delay(500);
CGNSPWR_1();
Delay(500);
del_All_SMS();
Delay(500);
p=NULL;
NVIC_EnableIRQ(TIM1_UP_IRQn);
while (1)
{
if (flag==0){
////waiting for +CMTI: from sim800
do {
p=strstr(str3,"+CGNSINF:");
}
while(!(strstr(str1,"+CMTI:")));
Delay(1000);
// sending AT+CMGR=1 command
CMGR();
Delay(2500);
flag=1;
if (flag==1) {
p=strstr(str1,"+CMGR");
j=strstr(str1,"loc");
if (p&&j){
CGNSINF();
Delay(300);
}
else
{
del_All_SMS();
flag=0;
}
p=strstr(str1,"+CGNSINF:");
if (p)
{
float a[5];
char str2[80];
const char s[2] = ",";
char *token;
// getting the lattitude and longitude
token = strtok(p, s);
for (int i=0;i<5;i++){
sprintf( str2," %s\n", token );
a[i]=atof(str2);
token = strtok(NULL, s);
}
sprintf(str2,"https://maps.google.com/?q=%.6f,%.6f",a[3],a[4]);
Send_SMS(str2);
p=NULL;
Delay(5000);
del_All_SMS();
flag=0;
for (int k=0;k<80;k++){
str2[k]=0;
}
}
}
}
}
}