cancel
Showing results for 
Search instead for 
Did you mean: 

Using multiple GPIO interupts with STM32L053 Nucleo board

johan2
Associate II
Posted on September 16, 2014 at 13:54

I am trying to use multiple interupts on my nucleo board. I have used the cube hal. My problem is that I dont get the interrupts generated on the PB0 pin, but the PB1 works ok.

I have tried to do the intialization in different order and it seems like it works better, but I dont understand why the HAL needs calls in a specific order.

My code to initialize the interrupts are based on the GPIO_EXTI example:

static void EXTI_Config(void)

{

  GPIO_InitTypeDef   GPIO_InitStructure;

  /* Enable GPIOB clock */

  __GPIOB_CLK_ENABLE();

  /* Configure PB0 pin  */

  GPIO_InitStructure.Mode = GPIO_MODE_IT_FALLING;

  GPIO_InitStructure.Pull = GPIO_PULLUP;

  GPIO_InitStructure.Pin = GPIO_PIN_0;

    GPIO_InitStructure.Speed = GPIO_SPEED_FAST;

  HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);

    

    

  /* Configure PB1 pin  */

  GPIO_InitStructure.Mode = GPIO_MODE_IT_FALLING;

  GPIO_InitStructure.Pull = GPIO_PULLUP;

  GPIO_InitStructure.Pin = GPIO_PIN_1;

  GPIO_InitStructure.Speed = GPIO_SPEED_FAST;

  HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);

    

  /* Enable and set EXTI  Interrupt to the lowest priority */

  HAL_NVIC_SetPriority(EXTI0_1_IRQn, 3, 0);

  HAL_NVIC_EnableIRQ(EXTI0_1_IRQn);

}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on September 18, 2014 at 12:39

Hello Johan,

Could you please let us know what was the working sequence & the non-working one?

Thanks

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on September 18, 2014 at 17:52

Hihedlund.johan,

Please find attached a GPIO_EXTI project using mutliple GPIO interrupts on PB0 and PB1 with the STM32L053 Nucleo board and the STM32Cube_FW_L0_V1.1.0 package available

http://www.st.com/web/en/catalog/tools/PF260508#

.

Let's try with this and keep us informed with your finding.

# Please extract atSTM32Cube_FW_L0_V1.1.0\Firmware\Projects\STM32L053R8-Nucleo\Examples\GPIO

Cheers,

Heisenberg.

________________

Attachments :

GPIO_EXTI_MUL.7z : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzZR&d=%2Fa%2F0X0000000bNh%2FK6hlu6yoDNmIu_rpjdKI1xQ21dB6IAR1hsuJedxK7E8&asPdf=false