Skip to main content
Associate III
Nov 15, 2024 9:06 AM UTC
Question

Use STM32F4 flash for non-volatile data storage (eeprom)

hello i am using stm32f429i-disc1 microcontroller board in this how to generate flash code (eeprom)

 


Your other thread showed a major confusion between what is a "microcontroller", and what is a "board" - so edited for clarity.

This topic has been closed for replies.

30 replies

Associate III
Nov 15, 2024 9:07 AM UTC

(duplicate thread - merged)

 

hello i am using stm32f429i-disc1 microcontroller board i want flash code (eeprom) for storing biomatric data

Andrew Neil
Super User
Nov 15, 2024 9:24 AM UTC

You mean you want to use the Flash for non-volatile data storage - "emulating" EEPROM?

For that, ST provide the STSW-STM32066 software pack, EEPROM emulation in STM32F40x/STM32F41x microcontrollers:

https://www.st.com/en/embedded-software/stsw-stm32066.html

See Application Note AN3969, EEPROM emulation in STM32F40x/STM32F41x microcontrollers for details:

https://www.st.com/en/embedded-software/stsw-stm32066.html#documentation

 

It may not exactly suit your requirements, but it does show how to use the STM32F4 Flash for data storage.

With that knowledge, you could adapt to your own needs; eg, see:
https://community.st.com/t5/stm32-mcus-embedded-software/eeprom-emulation-virtual-addresses/m-p/675964/highlight/true#M47888

and follow the link.

 

PS:

 


@syedhashmiraza wrote:

for storing biometric data


The nature of the data really makes no difference - it's all just data !

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Nov 18, 2024 9:27 AM UTC

@syedhashmiraza wrote:

this code is not build in stm32cubeide


how did you download from GitHub?

It's important to use git clone --recursive - the Zip download won't work:

https://community.st.com/t5/stm32-mcus/downloading-stm32cube-packages-from-github-correctly/ta-p/725288

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Nov 15, 2024 12:07 PM UTC

is STSW-STM32066  code work for stm32f4219i-disc1?

Associate III
Nov 16, 2024 6:21 AM UTC

(merged from duplicate thread)

 

hello iam using srm32f429i-disc1 microcontroller board and i want refrence code for emulated eeprom 

Visitor II
Nov 16, 2024 6:25 AM UTC

I think you have to use the STM32 HAL library. 

Associate III
Nov 16, 2024 6:59 AM UTC

yes iam using HAL library

Associate III
Nov 18, 2024 8:05 AM UTC

Hello,

I want to read and write string in eeprom  this is my code but in this code string is not storing in eeprom

 

#include "main.h"
#include <stdio.h>

/** @addtogroup EEPROM_Emulation
* @{
*/


/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/


/* Virtual address defined by the user: 0xFFFF value is prohibited */

uint16_t VirtAddVarTab[NB_OF_VAR] = {0x5555, 0x6666, 0x7777};

uint16_t VarDataTab[NB_OF_VAR] = {0, 0, 0};

uint16_t VarValue,VarDataTmp = 0;

/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void Error_Handler(void);

/* Private functions ---------------------------------------------------------*/

/**
* @brief Main program.
* None
* @retval None
*/

//char writeString[] = "Hello Hashmi";
char readString[64]={0};


int main(void)
{
	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
	HAL_Init();

	/* Configure the system clock to 180 MHz */
	SystemClock_Config();

	/* Unlock the Flash Program Erase controller */
	HAL_FLASH_Unlock();

	/* Configure LED3 */
	BSP_LED_Init(LED3);

	/* EEPROM Init */
	if( EE_Init() != EE_OK)
	{
		Error_Handler();
	}

	if((EE_ReadVariable(VirtAddVarTab[0], &readString[0])) != HAL_OK)
	{
		Error_Handler();
	}
	while(1)
	{
		char writeString[] = "Hello";
		for (int i = 0; i < sizeof(writeString); i++)
		{
			if (EE_WriteVariable(VirtAddVarTab[0] + i, (uint16_t*)&writeString[i]) != HAL_OK)
			{
				Error_Handler();
			}
		}
	}
}

 

 

 

mƎALLEm
ST Technical Moderator
Nov 18, 2024 10:49 AM UTC

Hello @syedhashmiraza 

Please don't duplicate the same subject on multiple threads. 

This thread will be merged with the previous one.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Nov 25, 2024 6:07 AM UTC

Again, please stop creating multiple threads on the same topic. Merged into original Thread.


 

hello in this code not storing string after power cut and poer on in eeprom not storing and in this code how to use printf?

 

 

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include <stdio.h>

/** @addtogroup EEPROM_Emulation
* @{
*/

/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/

/* Virtual address defined by the user: 0xFFFF value is prohibited */
uint16_t VirtAddVarTab[NB_OF_VAR] = {0x5555, 0x6666, 0x7777};
uint16_t VarDataTab[NB_OF_VAR] = {0, 0, 0};

uint16_t VarValue,VarDataTmp = 0;

/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void Error_Handler(void);

/* Private functions ---------------------------------------------------------*/

/**
* @brief Main program.
* None
* @retval None
*/

//char writeString[] = "Hello Hashmi";
char readString[64]={0};

int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();

/* Configure the system clock to 180 MHz */
SystemClock_Config();

/* Unlock the Flash Program Erase controller */
HAL_FLASH_Unlock();

/* Configure LED3 */
BSP_LED_Init(LED3);

/* EEPROM Init */
if( EE_Init() != EE_OK)
{
Error_Handler();
}

if (EE_ReadVariable(VirtAddVarTab[0], &VarDataTmp) != HAL_OK)
{
Error_Handler();
}

char writeString[] = "Hello";
for (int i = 0; i < sizeof(writeString); i++)
{
uint16_t charToWrite = (uint16_t)writeString[i];

// Pass the value, not the pointer
if (EE_WriteVariable(VirtAddVarTab[0] + i, charToWrite) != HAL_OK)
{
Error_Handler();
}
}

//printf("hello");
}

static void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
HAL_StatusTypeDef ret = HAL_OK;

/* Enable Power Control clock */
__HAL_RCC_PWR_CLK_ENABLE();

/* The voltage scaling allows optimizing the power consumption when the device is
clocked below the maximum system frequency, to update the voltage scaling value
regarding system frequency refer to product datasheet. */
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

/* Enable HSE Oscillator and activate PLL with HSE as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 360;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
ret = HAL_RCC_OscConfig(&RCC_OscInitStruct);
if(ret != HAL_OK)
{
while(1) { ; }
}

/* Activate the Over-Drive mode */
HAL_PWREx_EnableOverDrive();

/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
clocks dividers */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
ret = HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);
if(ret != HAL_OK)
{
while(1) { ; }
}
}

/**
* @brief This function is executed in case of error occurrence.
* None
* @retval None
*/
static void Error_Handler(void)
{
while(1)
{

/* Toggle LED3 fast */
BSP_LED_Toggle(LED3);
HAL_Delay(40);
}
}

#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

/* Infinite loop */
while (1)
{
}
}
#endif

/**
* @}
*/

 

mƎALLEm
ST Technical Moderator
Nov 25, 2024 8:49 AM UTC

Hello @syedhashmiraza ,

Please review tips on posting a thread in this community, especially for the following points:

- Title: "store" does not mean anything in the title needs to be short (not tooo short) and concise.

- Posting a code: you need to use </> button to paste your code.

- Part number: always state the FULL Part Number of the product used.

+

1- "hello in this code not storing string after power cut and poer on in eeprom not storing and in this code how to use printf?" -> not clear what do you mean by that. Need to elaborate more.

2- The thread subject is not related to CubeIDE usage but to the product usage -> To be moved to STM32 MCUs Products forum board.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Nov 25, 2024 11:13 AM UTC

You posted again the same question in a new thread which I moved to the forum archive.

Please don't duplicate threads! and keep the discussion in the same conversation until you solve your issue or you have another question.

Any further duplication will be moved to the archive.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.