Skip to main content
Boris Pokutinsky
Visitor II
November 22, 2017
Question

USB Video Class Host (UVC) into STM32xx HAL

  • November 22, 2017
  • 4 replies
  • 7579 views
Posted on November 22, 2017 at 18:06

Hi,

Actually the question is for ST. There are all examples and support of all USB host classes except just one - Video Class. I don't understand why it happens? Are there some road map to add it? 

And question to forum. 

May be someone can share UVC host (not device) driver for STM32 (L4 or F4 specifically) on HAL level? For my study I'm trying to connect to STM32L4 usb web cam, but I need to develop whole UVC host driver for it. 

May be someone can help with suggestions at least?

Thanks,

Boris

    This topic has been closed for replies.

    4 replies

    cable gu
    Associate II
    May 17, 2018
    Posted on May 17, 2018 at 04:23

    UVC is for vedio, and this need to many HW source, like SRAM, so I think this limit for the UVC to add the lib.

    iliasam
    Visitor II
    September 15, 2018
    Gavin Baker
    Associate III
    September 18, 2018

    UVC is a relatively large and complex device class. And for a host, it requires considerable bandwidth for video streams, memory for buffering frames, and CPU power for running codecs. Unless you have a very low-resolution FS webcam, it is unlikely that the L4 would be suitable match for this task. What exactly are you trying to implement?

    MKing
    Associate
    January 26, 2024

    Hi,

    it is a shame that CubeMX does not support a video class (uvc) for USB or a combination of several device classes. After one day of searching examples i found a "software pack" for CubeMX:

    alambe94/I-CUBE-USBD-Composite: Create STM32 USB Composite devices with ease. (github.com)

    here a small uvc example I created:

    mkoenig334455/-USB_Video_STM32F407VGTX: STM32F407VGTX + USB3310 example / enumerate as webcam and show 2 pictures as videostream (github.com) 

     

    ST, please support this project and promote it, so we all can save lifetime!

     

    MKing_0-1706259844317.png

     

     

    I use:

    CubeMX 6.10.0

    CubeIDE 1.14.0

    Processor: STM32F407VGT + PHY USB3310