USB CDC Port Not Shown In Device Manager(MCU STM32F!103RET6)
Hello Everyone,
Right now i am facing the issue on detection USB.I am attaching snap shots of the my USB configuration.
USB port not shown after powering up the board. i am doing some basic thing like on receiving via USB in RX interrupt function of USB i set one flag that will used in main function for further process.
Help Me if anyone knows the issue, i stuck here since 2 days.
STMCubeIDE Version:- 1.13.2
MCU:- STM32F103RET6
Debugger:- Jlink(4000Khz)
USB DP:- PA12
USB DM :-PA11
Internal Power Supply used which is given to MCU and other board peripheral.