Skip to main content
entwicklung
Associate III
August 7, 2015
Question

USB CDC CubeMX getting started

  • August 7, 2015
  • 4 replies
  • 1465 views
Posted on August 07, 2015 at 15:47

Hello friends,

I try to create a simple program, which uses a Virtual COM Port to send and receive data. As hardware I'm using a stm32f3discovery board. I already created the code with CubeMX and the devices shows up as Virtual COM in the device manager. Now I'm trying to use the functions placed in usbd_cdc_if.c I now, that I need to set the Buffer with data and then transmit.

mybuff[0] = 'A';
 USBD_CDC_SetTxBuffer(&hUsbDeviceFS, &mybuff[0], 8);
 CDC_Transmit(mybuff[],1);

But, as soon as I'm using the SetTxBuffer function in main, the Virtual COM disappears and the program seems to stop working. The question is: How can I simply realize send and receive data via the virtual COM? Are there any examples? Thanks in advance
    This topic has been closed for replies.

    4 replies

    Nesrine M_O
    Associate
    August 7, 2015
    Posted on August 07, 2015 at 17:16

    Hi,

    I suggest you to start from the example USB CDC under the STM32Cube_FW_F3_V1.2.0\Projects\STM32303C_EVAL\Applications\USB_Device\CDC_Standalone.

    -Syrine-

    entwicklung
    Associate III
    August 10, 2015
    Posted on August 10, 2015 at 11:11

    Thank you for this example, it is very similar to the code generated by CubeMX.

    Unfortunately I'm still not getting which function I need to send and receive data. I need some more detailed description to this code and how to use it. This are the functions I have in the usbd_cdc_if.c

    /* Private function prototypes -----------------------------------------------*/
    static
    int8_t CDC_Itf_Init (
    void
    );
    static
    int8_t CDC_Itf_DeInit (
    void
    );
    static
    int8_t CDC_Itf_Control (uint8_t cmd, uint8_t* pbuf, uint16_t length);
    static
    int8_t CDC_Itf_Receive (uint8_t* pbuf, uint32_t *Len);
    static
    void
    Error_Handler(
    void
    );
    static
    void
    ComPort_Config(
    void
    );
    static
    void
    TIM_Config(
    void
    );

    Nesrine M_O
    Associate
    August 10, 2015
    Posted on August 10, 2015 at 16:25

    Hi,

    In the usbd_cdc_interface.c file, you can find functions that ensure transmission and receive of data:

    When data are received over UART they are saved in the buffer ''UserTxBuffer''. Periodically, in a timer callback the state of the buffer ''UserTxBuffer'' is checked. If there are available data, they are transmitted by using this function: USBD_CDC_TransmitPacket()

    When data are received from PC host to STM32 device they are saved in the buffer ''UserRxBuffer'' then they are transmitted over UART using DMA mode: HAL_UART_Transmit_DMA()

    To make project functional into your discovery board you should modify your stm32f3xx_hal_msp.c (GPIO settings…)

    I suggest you also to read the readme file attached with the example in order to have more details about the project and how to use it.

    -Syrine-

    entwicklung
    Associate III
    August 11, 2015
    Posted on August 11, 2015 at 11:26

    Thank you again for this input, it put me in the right direction.

    I found out, that I need to use the functions CDC_Transmit_FS and CDC_Receive_FS Also I had to add some code:

    static
    int8_t CDC_Receive_FS (uint8_t* Buf, uint32_t *Len)
    {
    /* USER CODE BEGIN 7 */
    switch
    (Buf[0]){
    case
    'B'
    :
    CDC_Transmit_FS(Buf,1);
    break
    ;
    }
    USBD_CDC_ReceivePacket(&hUsbDeviceFS);
    return
    (USBD_OK);
    /* USER CODE END 7 */
    }
    uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
    {
    uint8_t result = USBD_OK;
    /* USER CODE BEGIN 8 */
    mcpy(UserTxBufferFS, Buf, 
    sizeof
    (
    char
    ) * Len);
    USBD_CDC_SetTxBuffer(&hUsbDeviceFS, UserTxBufferFS, Len); 
    result = USBD_CDC_TransmitPacket(hUsbDevice_0);
    /* USER CODE END 8 */
    return
    result;
    }

    I still have some problems to understand the receive function, but at least its working.