Skip to main content
Visitor II
August 31, 2023
Question

Unable to retrieve data from STM 32 board using pyserial

  • August 31, 2023
  • 4 replies
  • 1900 views

In this code, when I use the temp command, I always get output as "No response received." That means my python CLI is not receiving any data from the STM 32 board. But when I run the same command on the screen terminal on my mac, I get the data. What could the problem be?

I have ensured that the serial port configuration in my Python code (baud rate, data bits, stop bits, etc.) matches exactly with the configuration used when tested with screen.

 

 

 

import sys
import argparse
import configparser
import yaml
import serial
from rich import print

# Default values
DEFAULT_SERIAL_PORT = "/dev/cu.usbmodem14303"
BAUD_RATE = 115200

# Load configuration from the .ini file (if present)
config = configparser.ConfigParser()
config.read("config.ini")

# Override default values with values from the .ini file (if present)
serial_port = config.get("cli_params", "serial_port", fallback=DEFAULT_SERIAL_PORT)

# Parse command-line arguments
parser = argparse.ArgumentParser(description="My CLI Application")
parser.add_argument("--serial-port", type=str, default=serial_port, help="Serial port to use.")
args = parser.parse_args()

# Override values with command-line arguments
serial_port = args.serial_port

# Load commands from the YAML file
def load_commands(filename):
 with open(filename, "r") as file:
 commands_data = yaml.safe_load(file)
 
 commands = {}
 for cmd_data in commands_data.get("IES_module", []):
 cmd_name = cmd_data["Command"]
 commands[cmd_name] = cmd_data

 return commands

# Function to send a command to the STM32 board via serial
def send_command(serial_port, command):
 with serial.Serial(serial_port, BAUD_RATE, timeout=5) as ser:
 ser.write(command)

# Modify the receive_response function
def receive_response(serial_port, response_length=16):
 with serial.Serial(serial_port, BAUD_RATE, timeout=1) as ser:
 ser.flushInput() # Clear the input buffer
 response = ser.read(response_length) # Read the specified number of bytes
 return response

if __name__ == "__main__":
 try:
 # Load commands from the YAML file
 commands = load_commands("commands.yaml")

 # Print the available commands for the IES module
 print("Available commands for IES module:")
 print("Command | R/W | Notes")
 print("----------------------")
 for cmd_name, cmd_data in commands.items():
 print(f"{cmd_name} | 0x{cmd_data['ID']:02X} | {cmd_data['R/W']} | {cmd_data['Notes']}")

 while True:
 # Get the command from the user input or use a default command for testing purposes
 user_input = input("Enter command: ").strip().lower()

 if user_input == "exit":
 print("Exiting...")
 break
 
 # Check if the command exists in the commands dictionary
 if user_input not in commands:
 print(f"Invalid command: {user_input}")
 continue

 # Translate the command name to the command ID
 command_data = commands[user_input]
 command_id = command_data['ID']

 # Send the command to the STM32 board
 send_command(serial_port, bytes([command_id]))

 if user_input == "temp":
 response = receive_response(serial_port, response_length=16)
 if response:
 print(f"Received response (raw bytes): {response}")
 print(f"Response length: {len(response)} bytes")
 else:
 print("No response received.")

 else:
 response = receive_response(serial_port)
 if response:
 print(f"Received response (raw bytes): {response}")
 else:
 print("No response received.")

 except KeyboardInterrupt:
 print("\nExiting...")
 sys.exit(0)

 

 

 

I always get the output as "No response received." when the "temp" command is run.

This topic has been closed for replies.

4 replies

Explorer
March 18, 2024

@Xx11 I have the same issue - successful comms with screen, nothing with pyserial. Have you solved this?

Visitor II
February 27, 2025

I have a similar problem.

The following code only gets blank lines, presumably readline is timing out:

command = str.encode("{0}\n".format("ver"))
self.ser.write(command)
time.sleep(0.2)
for index in range(0,2):
 line = self.ser.readline()
 print(line)

When I open the same COM port with the same settings using Putty, typing in "ver" and enter works as expected.

What's interesting is that in the python code it appears that "ser.write" is working and the correct result is in the buffer. This is evident because if I run the Python then open the COM port with Putty, the first result I get when entering a command is actually the response that corresponded to the Python code. So the result is definitely in the buffer but for some reason ser.readline can't see it.

I've experimented with the STM32 code adding or removing the "\r" and "\n" and also using HAL_UART_Transmit instead of the printf wrapper for it.

It seems to be that the encoding from the STM32 is different in some way from the other times I've done this kind of thing. Previously in my work the device sending data on the uart was an FPGA, this is the first time I've tried it with the STM32 sending the data.

Pavel A.
February 27, 2025

Does your UART have hardware flow control?

 

Visitor II
February 27, 2025

I figured my issue out after some searching and experimenting.

Instead of \n in the command to write it needs to be \r. So line 1 changes in my code snippet

 

command = str.encode("{0}\r".format("ver"))
self.ser.write(command)
time.sleep(0.2)
for index in range(0,2):
 line = self.ser.readline()
 print(line)

. 

I don't see you appending anything to your command. Perhaps try appending that \r so the STM32 knows an entry is made.