Skip to main content
AMele.1
Visitor II
March 4, 2020
Question

UART LIN DMA HAL

  • March 4, 2020
  • 0 replies
  • 908 views

Hello, second day try to launch UART in LIN mode.

Task: waiting break, when break flag set up, switch on DMA receiver.

Transmitter works fine and send 100us break before frame.

But receiver can't set UP Break Flag.

And there are not everywhere examples =(

UART initialization:

void MX_USART2_UART_Init(void)
{
 
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_LIN_Init(&huart2, UART_LINBREAKDETECTLENGTH_10B) != HAL_OK)
 {
 Error_Handler();
 }
	__HAL_UART_ENABLE_IT(&huart2, UART_IT_LBD);
	HAL_UART_Receive_DMA(&huart2,(uint8_t*)UART2_RxBuffer,UART2_RX_BUFFER_SIZE);
}

DMA + GPIO initialization:

__HAL_RCC_USART2_CLK_ENABLE();
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**USART2 GPIO Configuration 
 PA2 ------> USART2_TX
 PA3 ------> USART2_RX 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* USART2_RX Init */
 hdma_usart2_rx.Instance = DMA1_Channel6;
 hdma_usart2_rx.Init.Request = DMA_REQUEST_2;
 hdma_usart2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_usart2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_usart2_rx.Init.MemInc = DMA_MINC_ENABLE;
 hdma_usart2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_usart2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_usart2_rx.Init.Mode = DMA_NORMAL;
 hdma_usart2_rx.Init.Priority = DMA_PRIORITY_LOW;
 if (HAL_DMA_Init(&hdma_usart2_rx) != HAL_OK)
 {
 Error_Handler();
 }
 
 __HAL_LINKDMA(uartHandle,hdmarx,hdma_usart2_rx);
 
 /* USART2 interrupt Init */
 HAL_NVIC_SetPriority(USART2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(USART2_IRQn);

Interrupt and launch DMA

void USART2_IRQHandler(void)
{
 /* USER CODE BEGIN USART2_IRQn 0 */
	if(__HAL_UART_GET_FLAG(&huart2,UART_FLAG_LBDF))
	{
		HAL_UART_Receive_DMA(&huart2,(uint8_t*)UART2_RxBuffer,UART2_RX_BUFFER_SIZE);
		__HAL_UART_CLEAR_FLAG(&huart2,UART_FLAG_LBDF);
		UART2_PacketReceived=true;		
	}
 /* USER CODE END USART2_IRQn 0 */
 HAL_UART_IRQHandler(&huart2);
 /* USER CODE BEGIN USART2_IRQn 1 */
 
 /* USER CODE END USART2_IRQn 1 */
}

Main:

 while (1)
 {
 /* USER CODE END WHILE */
		if(UART2_PacketReceived==true)
		{
		__HAL_UART_DISABLE_IT(&huart2, UART_IT_LBD);
			HAL_Delay(10);
			HAL_UART_DMAStop (&huart2);
			UART2_PacketReceived=false;
			__HAL_UART_ENABLE_IT(&huart2, UART_IT_LBD);
		}
 /* USER CODE BEGIN 3 */
 }

Currently interrupt work, DMA also work but UART receiver lost a lot of bytes or skip a lot of frames.

Please help me :sad_but_relieved_face:

This topic has been closed for replies.