Skip to main content
Senior
Aug 21, 2024 8:00 AM UTC
Solved

The purpose of the 'if ((hspi->hdmatx->Mode & DMA_LINKEDLIST) == DMA_LINKEDLIST)' in STM32U5 SPI transfer with DMA APIs

Hi,

I'm trying to combine the SPI and GPDMA on STM32U5. In the various SPI transfer APIs with suffix '_DMA', I can see the code below:

 /* Enable the Tx DMA Stream/Channel */
 if ((hspi->hdmatx->Mode & DMA_LINKEDLIST) == DMA_LINKEDLIST)
 {
 if (hspi->hdmatx->LinkedListQueue != NULL)
 {
 /* Set DMA data size */
 hspi->hdmatx->LinkedListQueue->Head->LinkRegisters[NODE_CBR1_DEFAULT_OFFSET] = hspi->TxXferCount;

 /* Set DMA source address */
 hspi->hdmatx->LinkedListQueue->Head->LinkRegisters[NODE_CSAR_DEFAULT_OFFSET] = (uint32_t)hspi->pTxBuffPtr;

 /* Set DMA destination address */
 hspi->hdmatx->LinkedListQueue->Head->LinkRegisters[NODE_CDAR_DEFAULT_OFFSET] = (uint32_t)&hspi->Instance->TXDR;

 status = HAL_DMAEx_List_Start_IT(hspi->hdmatx);
 }
 else
 {
 status = HAL_ERROR;
 }
 }
 else
 {
 status = HAL_DMA_Start_IT(hspi->hdmatx, (uint32_t)hspi->pTxBuffPtr, (uint32_t)&hspi->Instance->TXDR,
 hspi->TxXferCount);
 }

It seems the code try to support the 'DMA_LINKEDLIST' mode. But can't find a way to set it to 'DMA_LINKEDLIST' in the .ioc file. So, how ST expect us to use this mode?

Thanks.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Aug 21, 2024 9:14 AM UTC

Hello @diverger ,

You can specify the DMA_LINKEDLIST mode through GPDMA1 Mode and configuration on STM32CubeMX (please see attachment files).
The Execution Mode can be: Circular or Linear (By Default) 

  • Circular Mode :

 

handle_GPDMA1_Channel15.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
#define DMA_LINKEDLIST_CIRCULAR (DMA_LINKEDLIST | (0x01U)​

 

  • Linear Mode :

 

handle_GPDMA1_Channel15.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_NORMAL;
#define DMA_LINKEDLIST_NORMAL DMA_LINKEDLIST​

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Aug 21, 2024 9:14 AM UTC

Hello @diverger ,

You can specify the DMA_LINKEDLIST mode through GPDMA1 Mode and configuration on STM32CubeMX (please see attachment files).
The Execution Mode can be: Circular or Linear (By Default) 

  • Circular Mode :

 

handle_GPDMA1_Channel15.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
#define DMA_LINKEDLIST_CIRCULAR (DMA_LINKEDLIST | (0x01U)​

 

  • Linear Mode :

 

handle_GPDMA1_Channel15.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_NORMAL;
#define DMA_LINKEDLIST_NORMAL DMA_LINKEDLIST​

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Aug 27, 2024 2:30 PM UTC

Hi @diverger ,

Did the solution shared solve your problem?

I'll be waiting for your feedback :) 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks