Skip to main content
JAN R
Associate III
August 15, 2018
Question

STOP mode and STM32L152~ 440 uA

  • August 15, 2018
  • 2 replies
  • 731 views

Dear,

I have Nucelo board with STM32L152RE. I have just made a simple project with CubeMX:

After reset - blink 5 times by LED and then go to STOP mode. After pushing a button repeat whole proces again and again. Button is on EXTI13.

My problem is that power consumption is about 440 uA and I can not reach better results. (MY nucleo is in original state - no external parts are connected).

My SYSCLK is MSI with 2.097 MHz

Can you help me with power consumption please?

Thank you very much. Jan.

int main(void)
{
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 
 while (1)
 {
	 for(uint8_t i=0;i<5;i++)
	 {
		 LL_GPIO_TogglePin(LD2_GPIO_Port,LD2_Pin);
		 LL_mDelay(200);
	 }
 
 /* disable Systick timer */
	 SysTick->CTRL &=~ SysTick_CTRL_ENABLE_Msk;
 
 /*Set all pins as analog*/
	 LL_GPIO_InitTypeDef gpio_initstruct = {LL_GPIO_PIN_ALL, LL_GPIO_MODE_ANALOG,
				 LL_GPIO_SPEED_FREQ_HIGH, LL_GPIO_OUTPUT_PUSHPULL,
				 LL_GPIO_PULL_NO, LL_GPIO_AF_0};
 
	 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA |
			 LL_AHB1_GRP1_PERIPH_GPIOB |
			 // LL_AHB1_GRP1_PERIPH_GPIOC | 
			 LL_AHB1_GRP1_PERIPH_GPIOD |
			 LL_AHB1_GRP1_PERIPH_GPIOE |
			 LL_AHB1_GRP1_PERIPH_GPIOF |
			 LL_AHB1_GRP1_PERIPH_GPIOG |
			 LL_AHB1_GRP1_PERIPH_GPIOH);
 
			 LL_GPIO_Init(GPIOA, &gpio_initstruct);
			 LL_GPIO_Init(GPIOB, &gpio_initstruct);
			 // LL_GPIO_Init(GPIOC, &gpio_initstruct); /* because of EXTI - button to wakeup*/
			 LL_GPIO_Init(GPIOD, &gpio_initstruct);
			 LL_GPIO_Init(GPIOE, &gpio_initstruct);
			 LL_GPIO_Init(GPIOF, &gpio_initstruct);
			 LL_GPIO_Init(GPIOG, &gpio_initstruct);
			 LL_GPIO_Init(GPIOH, &gpio_initstruct);
 
			 LL_AHB1_GRP1_DisableClock(LL_AHB1_GRP1_PERIPH_GPIOA |
			 LL_AHB1_GRP1_PERIPH_GPIOB |
			 // LL_AHB1_GRP1_PERIPH_GPIOC | /* because of EXTI - button to wakeup*/
			 LL_AHB1_GRP1_PERIPH_GPIOD |
			 LL_AHB1_GRP1_PERIPH_GPIOE |
			 LL_AHB1_GRP1_PERIPH_GPIOF |
			 LL_AHB1_GRP1_PERIPH_GPIOG |
			 LL_AHB1_GRP1_PERIPH_GPIOH);
 
		 /* Enable Power Clock */
		LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
 
		LL_PWR_EnableUltraLowPower();
 
		LL_PWR_SetRegulModeLP(LL_PWR_REGU_LPMODES_LOW_POWER);
 
		LL_PWR_SetPowerMode(LL_PWR_MODE_STOP);
 
		LL_LPM_EnableDeepSleep();
		
 __WFI();
	
 //HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);
	 
 /*enable Systick after wakeup*/
 SysTick->CTRL |= SysTick_CTRL_ENABLE_Msk;
 
	 MX_GPIO_Init();
 }
 }

This topic has been closed for replies.

2 replies

RN_it
Associate III
August 22, 2018

try with analog mode for all the unused GPIOC pins.

JAN R
JAN RAuthor
Associate III
September 11, 2018

Thank you, but I tried it, Every single pin is set as Analog....