Skip to main content
Gaston
Associate III
July 2, 2024
Question

STMG0 Multichannel ADC CubeIDE configuration issue

  • July 2, 2024
  • 3 replies
  • 2124 views

Hi,

I'm not able to set the STM32G030C6 ADC1 for 9 + Internal Temperature Sensor channels. Here's my ADC1 Mode and Configuration parameters

 

Gaston_1-1719938564685.png

Gaston_2-1719938744194.png

I'm using this recently updated Software Package Version

STM32CubeG0 Firmware Package V1.6.2

Does anyone know what the problem is?

Regards,
Gaston

This topic has been closed for replies.

3 replies

KnarfB
Super User
July 2, 2024

no such errors here with STM32CubeMX 6.11.1. Conflicts with other peripherals?

Screenshot 2024-07-02 195740.png

Gaston
GastonAuthor
Associate III
July 2, 2024

No. It does not work with latest CubeIDE v1.16 (CubeMX v6.12) update.

I've downgraded the iDE to v1.15.2 (CubeMX 6.11.1) and it works fine.

It seems a CubeIDE v1.16 issue

Associate
July 5, 2024

Hi. Same problem here. It seems to have something to do with setting the sequencer to not fully configurable.

I've started a new clean project, STM32G070RBTx, only configure one pin on the ADC tab, set sequencer to not fully configurable, and the error appears

EdwinID_0-1720185024725.png

Regards,

Edwin