Skip to main content
Associate III
May 28, 2024
Solved

STM32U5A5QJI6Q Reference Design - Reg

  • May 28, 2024
  • 4 replies
  • 2784 views

 

 

Hi Team,

I am reaching out to inquire about the availability of the reference design for the STM32U5A5QJI6Q microcontroller

 We are currently in the process of designing a project that could greatly benefit from utilizing this specific microcontroller and having access to its reference design would be immensely helpful in our development process.

Could you please provide information on how we can obtain the reference design for the STM32U5A5QJI6Q? Additionally, any accompanying documentation or resources related to the design would be greatly appreciated.

 

Regards

Sathiya

This topic has been closed for replies.
Best answer by STTwo-32

Hello @Sakthi_IND 

You can find here all CAD Resources available for the STM32U5A5QJI6Q MCU. The Schematics are available for boards designs only. This MCU is not implemented on any one of our evaluation boards. for more details about the design of a board based on an STM32U5, you can follow the AN5373.

Best Regards.

STTwo-32

 

4 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 28, 2024

Hello @Sakthi_IND 

You can find here all CAD Resources available for the STM32U5A5QJI6Q MCU. The Schematics are available for boards designs only. This MCU is not implemented on any one of our evaluation boards. for more details about the design of a board based on an STM32U5, you can follow the AN5373.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
May 28, 2024

Hi,

Thank you for your response, is available only the schematics.

Regards,

Sathiya

Associate III
May 29, 2024

Hi,

We are currently in the process of selecting components for our project, and we have identified the STM32U5A5QJ9(STM32U5A5QJ, foot-print size UFBGA 132 7x7x0.6 P 0.5 mm) microcontroller as a potential candidate. However, upon reviewing the datasheet, we noticed that there are two variants available: one with SMPS (Switched-Mode Power Supply) and one without.

 

Could you please provide clarification on the differences between these two variants? Specifically, we would like to understand the functionality and features that differentiate the STM32U5A5QJ variant with SMPS from the one without SMPS.

Additionally, as we are interested in procuring the exact variant that suits our project requirements, could you please advise on how we can accurately specify and order the desired variant online?

Which variant is suitable for a wearable device (battery powered)?

Regards,

Sathiya