As said @STOne-32, This is the ST-Link ( debugger) driver and not the main MCU. You can stop this pop up only using your PC USB ports internal configurations.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Probably going to want a board where USB is connected to the L476 and not F103 if you want to work on USB Device firmwares. Or use the NUCLEO-144 family, or DISCO boards
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
@Ephraimoved If this popup disturbs you - open the Device Manager in Windows, find this thing under Disk Drives and disable it. Ask you IT at work to help, if not sure.
Also, there are advices to run the ST-Link firmware updater and disable this "disk drive" - but this can break some old software. Try this on your own risk. Disabling the "disk" in device manager is quick and safe, no touching the ST-Link firmware.