Skip to main content
Yan Rosh
Associate II
September 12, 2019
Question

STM32H753AI Recommended Footprint

  • September 12, 2019
  • 3 replies
  • 1667 views

Hello,

In the STM32H753AI datasheet, there are footprint guidelines for all the packages, except for the UFBGA169 (see attached image).

Has anyone built a board with this package? Where did you find any info on this type of package?

Is there a database of ST footprints I can look at to find this info?

In a similar question, one of the answers led to AN4938 (Getting started with hardware dev....), but there is no specific package information there either...

Thanks in advance,

Yan

This topic has been closed for replies.

3 replies

Danish1
Lead III
September 12, 2019

stm32l4a6 has a similar UFBGA169 package, and I see it's data-sheet has a recommended footprint for a single pad, which is more than you got in your data sheet. Maybe you could build something from that?

But I think this is something you will have to discuss with your pcb house.

I have resorted to stacked via-in-pad to route enough tracks out of an ST WLCSP100 package. Not cheap but I couldn't see how to get the inner tracks out.

Hope this helps,

Danish

Yan Rosh
Yan RoshAuthor
Associate II
September 14, 2019

Thanks for the answer, I saw that datasheet as well, just wanted to make sure that it's indeed the same package...

Yan

Amel NASRI
ST Technical Moderator
September 27, 2019

Hi @Yan Rosh​ ,

A request is tracked internally to add "UFBGA169 recommended footprint" for STM32H7 datasheets where this package is available.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.