Skip to main content
Associate III
May 24, 2024
Solved

[STM32H750XBH6] Output current Question

  • May 24, 2024
  • 3 replies
  • 2081 views

Hello,

I use STM32H750XBH6, DataSheet 'Absolute maximum ratings' say that 'Output current sunk by Px_C pins' is 1mA

微信截图_20240524114156.jpg

What does Px C mean?

Does it mean all the pins of GPIOC?

Or something else?

 

Thanks!

This topic has been closed for replies.
Best answer by Peter BENSCH

Px_C does not stand explicitely for Port C, but for special pins that are additionally led out in order to have direct access to the analogue functions. As it happens, in the case of the STM32H750 some of them are part of Port C, are labelled PC2_C or PC3_C and are alternatives with an additional switch to the PC2 and PC3 pins.

Please see RM0433, section 11.3.13, e.g. fig 76 for more information.

Hope that helps?

Regards
/Peter

3 replies

PasserbyAuthor
Associate III
May 24, 2024

@mƎALLEm 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 24, 2024

Px_C does not stand explicitely for Port C, but for special pins that are additionally led out in order to have direct access to the analogue functions. As it happens, in the case of the STM32H750 some of them are part of Port C, are labelled PC2_C or PC3_C and are alternatives with an additional switch to the PC2 and PC3 pins.

Please see RM0433, section 11.3.13, e.g. fig 76 for more information.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PasserbyAuthor
Associate III
May 24, 2024

Hello , @Peter BENSCH 

         Thanks for your reply!