Skip to main content
BWolf.1
Associate
July 13, 2022
Solved

STM32H745 (LQFP144): can pin PF10 be used as a single-ended ADC channel using ADC3_INP6 ?

  • July 13, 2022
  • 2 replies
  • 1100 views

Same question for pin PF14: can it be used as a single-ended ADC channel using ADC2_INP6 ?

The Cube does not indicate if these pins can be used as single-ended ADC channels.

Thank you.

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome, @BWolf.1​, to the community!

We are sorry for any confusion this may cause, but IN6 (marked as INP6 in pinout view) is a single-ended input. It may be a little confusing that inputs like IN11 or IN14 are explicitly marked single-ended, which is just a left over from other derivatives in other packages of the same family where you can select differential and single-ended for the pin.

Summary: even if it is not explicitly marked single-ended on an ADC input - if it has no drop-down menu and can only be selected with a tick, then it is a single-ended input.

Does it answer your question?

Regards

/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
July 13, 2022

Welcome, @BWolf.1​, to the community!

We are sorry for any confusion this may cause, but IN6 (marked as INP6 in pinout view) is a single-ended input. It may be a little confusing that inputs like IN11 or IN14 are explicitly marked single-ended, which is just a left over from other derivatives in other packages of the same family where you can select differential and single-ended for the pin.

Summary: even if it is not explicitly marked single-ended on an ADC input - if it has no drop-down menu and can only be selected with a tick, then it is a single-ended input.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BWolf.1
BWolf.1Author
Associate
July 13, 2022

Hi Peter,

That answers my question. Great!

Thank you very much.