Skip to main content
eeyurdakul
Associate II
June 30, 2021
Question

STM32H7 SDMMC2 DMA Configuration

  • June 30, 2021
  • 1 reply
  • 2354 views

I can configure MDMA for SDMMC1 in STM32H730 in STM32CubeIDE.

But I do not understand how to enable it for SDMMC2.

In the documentation it says SDMMC2 has a direct access to DMA1 & DMA2. But I could not see it in DMA configuration panel.

Could you help me about this issue please?

0693W00000BcPf9QAF.jpg

This topic has been closed for replies.

1 reply

Bowman32
ST Employee
July 13, 2021

Hi @eeyurdakul​ 

The SDMMC has an embedded DMA (internal direct memory access, IDMA) and no need for an external DMA.

You can refer to application note AN5200 "Getting started with STM32H7 Series SDMMC host controller"

Also you can refer to STM32CubeH7 firmware examples via this path: STM32Cube_FW_H7_V1.8.0\Projects\STM32H735G-DK\Examples\SD.

Best regards,

Bouraoui