Solved
STM32H7 SAI / I2S max input clock "sai_x_ker_ck"
Hello,
what is the maximum input clock for the SAIs and I2Ss for the H7 ?
I mean "sai_x_ker_ck" and "spi_ker_ck".
I couldn't find it in neither RM nor DS.
Is it dependent on some AHB / APB or D1/2/3 clock?
98.304 MHz is working (it is also in the RM's examples), even when abusing it to create a sample rate of 384 kHz.