Question
stm32h7 pin configuration tool
Posted on October 31, 2017 at 13:53
I'm a circuit board designer and I've been given a set of requirements to map a given set of functions out of the STM32H7. Is there a pin configuration tool that allows a user to specify which functions (CAN, ULPI, SDHC, etc...) are desired and it will map out the necessary pins? It's a pain to keep flipping through the datasheet and trying to map it on an Excel spreadsheet, I get one set up and then it's got to move so I can map another bus.