Skip to main content
Danilo Frigerio
Associate
May 7, 2018
Solved

STM32H7 GPIO TOGLE MAX FREQUENCY

Posted on May 07, 2018 at 14:08

With STM32F765 and MDK-ARM compiler ( O3 and compile for SPEED I was able to achieve 108Mhz on output pin, performing while loop ( just main() and all interrupt disabled ) .

Now with STM32H743 with same compiler and same source maximum frequency is 16.7MHz , with PLL configured to have 400MHz clock ( tested on RCC_MCO2 output pin )

Anyone know why ?

Thanks

    This topic has been closed for replies.
    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    May 17, 2018
    Posted on May 17, 2018 at 15:38

    Hi

    Frigerio.Danilo

    ‌,

    First, we may ask about the relevance of toggling a GPIO with CPU at maximum clock (as stated by Avatar)?

    For some use-cases, you may use a timer ...

    Back to the explanation of the discrepancy between results with STM32F7 and the ones with STM32H7: the main reason is that both families don't share the same architecture:

    • STM32F7 has one bus matrix and both the Core and and GPIO are connected to that same bus matrix
    • STM32H7 has three domains.Cortex-M7 is connected to AXI bus matrix while the GPIO is connected to another AHB bus matrix. Then, a latency is introduced because of bridges connecting these bus matrices.

    You may refer to 'System Architecture' section in the reference manuals of both products for more details.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

    4 replies

    henry.dick
    Associate II
    May 7, 2018
    Posted on May 07, 2018 at 16:42

    Default clock, bus speed, gpio drive, compiler optimization, software access approach, coding, .... 

    AvaTar
    Senior III
    May 7, 2018
    Posted on May 07, 2018 at 16:57

    GPIO glitch filter.

    WTH is the relevance of toggling a pin with 100% core load ?

    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    May 17, 2018
    Posted on May 17, 2018 at 15:38

    Hi

    Frigerio.Danilo

    ‌,

    First, we may ask about the relevance of toggling a GPIO with CPU at maximum clock (as stated by Avatar)?

    For some use-cases, you may use a timer ...

    Back to the explanation of the discrepancy between results with STM32F7 and the ones with STM32H7: the main reason is that both families don't share the same architecture:

    • STM32F7 has one bus matrix and both the Core and and GPIO are connected to that same bus matrix
    • STM32H7 has three domains.Cortex-M7 is connected to AXI bus matrix while the GPIO is connected to another AHB bus matrix. Then, a latency is introduced because of bridges connecting these bus matrices.

    You may refer to 'System Architecture' section in the reference manuals of both products for more details.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Danilo Frigerio
    Associate
    May 17, 2018
    Posted on May 17, 2018 at 16:00

     ,

     ,

    Dear Amel

    What you said is about what I imagined, really I don't need to toggle

    pin at this speed, this was just to compare M7 and H7.

    I will compare it in a real way, comparing my fw now running on

    STM32F765 ( high speed camera scanning )

    Thanks and regards

    Danilo Frigerio

    Il 17/05/2018 15:38, Amel N ha scritto:

    >,

    STMicroelectronics Community

    <,https://community.st.com/?et=watches.email.thread>,

    >,

    Re: STM32H7 GPIO TOGLE MAX FREQUENCY

    reply from Amel N

    <,

    /STM32 MCUs Forum/ - View the full discussion

    <,https://community.st.com/0D70X000006Sm8qSAC

    >,