Skip to main content
Associate II
November 18, 2025
Solved

STM32H573V UCPD CC2 and PC9 interference

  • November 18, 2025
  • 3 replies
  • 152 views

HI,

I am working on a board using STM32H573V and have a working solution with UCPD detecting an inserted memory stick and running the MSC class. In an other part of the software I am using PC9 as an GPIO push-pull, low speed output and as soon as I set it to high, the voltage at PB14 (UCPD CC2) drops from 3.3V to 1.5V and my UCPD handler signals a device attached and turns VBUS on even though nothing is attached. There is no other electrical connection between PC9 and PB14 on the board. I am using a TCPP03-M20 for VBUS switching. The board is acting as VBUS source.

Best answer by waclawek.jan

PC9 is UCPD1_DB2 i.e. part of the dead-battery mechanism ; and as such, gates the pull-down at PB14=UCPD1_CC2.

Set PWR_UCPDR.UCPD_DBDIS bit to disable this behaviour.

JW

3 replies

waclawek.jan
waclawek.janBest answer
Super User
November 18, 2025

PC9 is UCPD1_DB2 i.e. part of the dead-battery mechanism ; and as such, gates the pull-down at PB14=UCPD1_CC2.

Set PWR_UCPDR.UCPD_DBDIS bit to disable this behaviour.

JW

DirkHAuthor
Associate II
November 18, 2025

Thank you for the swift reply, Jan ! Problem solved :))

PR.10
Associate III
January 26, 2026

For future developers having the same wtf moments.
You can call HAL_PWREx_DisableUCPDDeadBattery(), write the registers directly or there is actually a checkbox in the IDE that would saved me hours of investigating ;)

PR10_0-1769460620554.png

 

SThom.7
Associate III
March 19, 2026

why is that not made more clear by ST, or better yet disabled by default if you are not using USB!? Not even Cube does this.

I have had a problem on STM32H562 with PB14 (UCPD1_CC2 - FT_c) configured as an open drain output.

the output was not always at the correct level and switching erratically somehow related to QSPI access.

calling HAL_PWREx_DisableUCPDDeadBattery() has fixed the problem.

 

this from the HAL drivers should really be made more clear and explicit elsewhere?

/**
* @brief Disable dead battery behavior.
* @note After exiting reset, the USB Type-C (dead battery) behavior is
* enabled, which may have a pull-down effect on CC1 and CC2 pins.
* It is recommended to disable it in all cases, either to stop this
* pull-down or to handover control to the UCPD (the UCPD must be
* initialized before doing the disable).
* @retval None.
*/
void HAL_PWREx_DisableUCPDDeadBattery(void)