cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F723 DISCO, Audio play/record example - SAI interrupts twice fast then expected

BRusl.1
Associate III

Hi,

Having STM32F723 DISCO with simple play/record example. Need to process sound by 20ms periods, so I've calculated PCM buffer size as :

```

#define AUDIO_CHANNELS         2

#define AUDIO_PCM_BIT_RESOLUTION    16

#define AUDIO_SAMPLE_LENGTH_MS     20

#define AUDIO_SAMPLE_SIZE        (AUDIO_CHANNELS * (SAMPLE_RATE/1000) * AUDIO_SAMPLE_LENGTH_MS)

#define AUDIO_PERIODS          2

#define AUDIO_BUFFER_SIZE        (AUDIO_SAMPLE_SIZE * AUDIO_PERIODS)

```

So I'm expect the HAL_SAI_TxHalfCpltCallback & HAL_SAI_TxCpltCallback to trigger each 20ms, but it triggers each 10ms:

```

[0000:00:00:00.000] Firmware v1.0 started, h/w rev: 0x1000

[0000:00:00:00.000] System clock: 216 MHz, HCLK/AHB clock: 216 MHz, PCLK1/APB1 clock: 54 MHz, PCLK2/APB2 clock: 108 MHz

[0000:00:00:00.655] SAI clock: 49.142856 MHz

[0000:00:00:00.655] Audio inited: Sample rate: 16000, channels: 2, period length: 20 ms, AUDIO_PCM16BIT_SAMPLE_SIZE: 640, doubled AUDIO_PCM16BIT_BUFFER_SIZE: 1280

[0000:00:00:00.655] Board inited

[0000:00:00:00.655] App started

[0000:00:00:00.655] Generating sine table for 200Hz

[0000:00:00:00.832] Sine table gen completed

[0000:00:00:00.833] Audio started

[0000:00:00:00.843] BSP_AUDIO_OUT_HalfTransfer_CallBack

[0000:00:00:00.853] BSP_AUDIO_OUT_TransferComplete_CallBack

[0000:00:00:00.863] BSP_AUDIO_OUT_HalfTransfer_CallBack

[0000:00:00:00.873] BSP_AUDIO_OUT_TransferComplete_CallBack

```

What can be the problem ?

This discussion is locked. Please start a new topic to ask your question.
17 REPLIES 17
BRusl.1
Associate III

If I change SlotInit.SlotNumber to 2 then I'm having correct 20 ms interrupts :

```

[0000:00:00:00.552] BSP_AUDIO_OUT_HalfTransfer_CallBack

[0000:00:00:00.572] BSP_AUDIO_OUT_TransferComplete_CallBack

```

But TP7 (SAI2_SCK_A) is still shows 1.025Mhz and now no sound at all. The SAI_I2S_STANDARD do not change anything here.

BRusl.1
Associate III

I do not touch WM8994 modes - all left as is from stm32f723e_discovery_audio.c

BRusl.1
Associate III

Found the issue, I've called the :

```

if (BSP_AUDIO_OUT_Init((spk ? OUTPUT_DEVICE_SPEAKER : OUTPUT_DEVICE_HEADPHONE), AUDIO_DEFAULT_VOLUME, SAMPLE_RATE))

 return AUDIO_ERROR_IO;

if (BSP_AUDIO_IN_Init(SAMPLE_RATE, AUDIO_PCM_BIT_RESOLUTION, AUDIO_CHANNELS))

 return AUDIO_ERROR_IO;

```

But looks like BSP_AUDIO_IN_Init mangles the SAI settings, if I comment out the BSP_AUDIO_IN_Init() then playback work as expected !

Seems like full duplex was never tested or intented in stock BSP code ;(

Thanks AScha for pointing out to the problem, though I still do not understand how it is working with SAI2_SCK_A 1.025Mhz

AScha.3
Super User

1M because 4 slot (= channels) are sent, but only 2 filled with data, 2 slots as dummy (null filled);

so 64 b in a frame, but 32 b (2 x 16 b ) is the real data.

If you feel a post has answered your question, please click "Accept as Solution".
BRusl.1
Associate III

BTW: with SAI_SLOT_NUMBER set to 2 speaker output no longer works (silence) but headphone is ok.

BRusl.1
Associate III

I've hoped that stock example is something that should work and tested at factory with all outputs, sample rates, etc. but seems this is just buggy skeleton code

AScha.3
Super User

oh, its STM standard.... :)

If you feel a post has answered your question, please click "Accept as Solution".
BRusl.1
Associate III

They are always using 4 slots - 2 for speaker, 2 for headphone, I think this is for having the same SAI config for OUTPUT_DEVICE_BOTH mode. Next I've found the BSP_AUDIO_IN_OUT_Init() which works at least for 4 slots. Thanks AScha for your help again !