STM32F7 USB Device Not Recognized as Virtual COM Port (VCP)
- 8 replies
- 4159 views
Hello everyone,
I’m working on an STM32F7 project where I’m trying to establish USB communication between my STM32F746 Discovery board and a PC. I am really new at this really first time. I have configured the board for USB_OTG_FS in STM32CubeMX, and I’m trying to use it as a Virtual COM Port (VCP). However, when I connect the board to the PC using the USB_FS port, it’s not being recognized as a COM port or any device at all in the Device Manager.
The only time I see a COM port is when I connect the ST-Link USB, which shows up as a Virtual COM Port. I have already:
- Enabled the USB_DEVICE in STM32CubeMX and selected the CDC class.
- Generated the code and set up the USB_DEVICE middleware.
- Tried with different USB cables to rule out a cable issue.
- Checked the board configuration, and the USB pins are correctly assigned.
Additionally, I configured the board to flash an LED to confirm it’s functioning, which works fine. My goal is to transfer files between the app I am currently developing and the STM32 board through USB.
I would really appreciate any suggestions or guidance on:
- Getting the board to show up as a VCP in the Device Manager.
- Troubleshooting USB enumeration issues.
Thanks in advance!