cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429I-DISCO - USART3 outputs only 1.6V

smrtkai
Senior

Hi everyone,

I am trying to get USART3 running on my STM32F429I-DISCO board. USART3 is configured with the following configurations:

  • Mode: Asynchronous
  • Hardware Flow Control: Disable
  • Baudrate: 115200, Word Length: 8, Stop Bits: 1
  • GPIO: PD8 = TX, PD9 = RX

I have tried a lot of different configurations. In every configuration I have tried so far, PD8 outputs only a 1.6V signal. The receiver expects a 3.3V signal.

What might cause the "low" voltage at PD8?

Kind regards,

Kai

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

High load from external circuitry, bad solder joint.

Make sure the onboard SDRAM does not drive its data lines.

JW

Manual says the pin is used by the SDRAM, so two things driving in different states.

https://www.st.com/content/ccc/resource/technical/document/user_manual/6b/25/05/23/a9/45/4d/6a/DM00093903.pdf/files/DM00093903.pdf/jcr:content/translations/en.DM00093903.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
smrtkai
Senior

Thank you!!!

I am not using the SDRAM and it is not initialized. I have generated the code with STM32CubeMX only with the USART configuration.

How can I get it working with 3.3V?

You might not be using it, but you're still dragging the boat anchor.

Desolder the unused SDRAM, or lift the specific pin.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..