stm32f411 tim5 and tim9 can not use to be TIM_Encoder mode
int main(void)
{
HAL_Init();
BSP_LED_Init(LED3);
BSP_LED_Init(LED4);
BSP_LED_Init(LED5);
BSP_LED_Init(LED6);
/* Initialize TIM3 to emulate a quadrature encoder outputs */
Init_TIM_Emulator(&EmulatorHandle);
UartHandle.Instance = USARTx;
UartHandle.Init.BaudRate = 9600;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
if(HAL_UART_Init(&UartHandle) != HAL_OK)
{
Error_Handler();
}
Encoder_Handle.Instance = TIM1;
Encoder_Handle.Init.Period = 65535;
Encoder_Handle.Init.Prescaler = 0;
Encoder_Handle.Init.ClockDivision = 0;
Encoder_Handle.Init.CounterMode = TIM_COUNTERMODE_UP;
Encoder_Handle.Init.RepetitionCounter = 0;
sEncoderConfig.EncoderMode = TIM_ENCODERMODE_TI12;
sEncoderConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
sEncoderConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
sEncoderConfig.IC1Prescaler = TIM_ICPSC_DIV1;
sEncoderConfig.IC1Filter = 0;
sEncoderConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
sEncoderConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
sEncoderConfig.IC2Prescaler = TIM_ICPSC_DIV1;
sEncoderConfig.IC2Filter = 0;
if(HAL_TIM_Encoder_Init(&Encoder_Handle, &sEncoderConfig) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
BSP_PB_Init(BUTTON_KEY, BUTTON_MODE_GPIO);
/* Wait for USER Button press before starting the Communication */
while (BSP_PB_GetState(BUTTON_KEY) == RESET)
{
/* Toggle LED3 waiting for user to press button */
BSP_LED_Toggle(LED3);
HAL_Delay(40);
}
/* Wait for USER Button to be release before starting the Communication */
while (BSP_PB_GetState(BUTTON_KEY) == SET)
{
}
/* Turn LED3 off */
BSP_LED_Off(LED3);
/* Start the encoder interface */
HAL_TIM_Encoder_Start(&Encoder_Handle, TIM_CHANNEL_ALL);
/* Infinite loop */
while (1)
{
/* Step 1: */
Emulate_Forward_Direction(&EmulatorHandle);
HAL_Delay(10);
/* Get the current direction */
uwDirection = __HAL_TIM_IS_TIM_COUNTING_DOWN(&Encoder_Handle);
uwcount = __HAL_TIM_GET_COUNTER(&Encoder_Handle);
TxBuffer[0] =(unsigned int)uwcount>>8 & 0xff;
TxBuffer[1] =(unsigned int)uwcount & 0xff;
TxBuffer[2]=uwDirection;
TxBuffer[3] =3;
TxBuffer[4] =4;
if(HAL_UART_Transmit(&UartHandle, (uint8_t*)TxBuffer, 5, 50)!= HAL_OK)
{
Error_Handler();
}
}
}
static void Init_TIM_Emulator(TIM_HandleTypeDef* htim)
{
/* Initialize TIM3 peripheral as follow:
+ Prescaler = 0
+ Period = 65535
+ ClockDivision = 0
+ Counter direction = Up
*/
htim->Instance = TIM3;
htim->Init.Period = EMU_PERIOD;
htim->Init.Prescaler = 0;
htim->Init.ClockDivision = 0;
htim->Init.CounterMode = TIM_COUNTERMODE_UP;
if(HAL_TIM_OC_Init(htim) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*## Configure the Output Compare channels #########################################*/
/* Output Compare Toggle Mode configuration: Channel1 */
sConfig.OCMode = TIM_OCMODE_TOGGLE;
sConfig.Pulse = (EMU_PERIOD * 1 )/4;
sConfig.OCPolarity = TIM_OCPOLARITY_LOW;
if(HAL_TIM_OC_ConfigChannel(htim, &sConfig, TIM_CHANNEL_1) != HAL_OK)
{
/* Configuration Error */
Error_Handler();
}
/* Output Compare Toggle Mode configuration: Channel2 */
sConfig.Pulse = (EMU_PERIOD * 3 )/4;
if(HAL_TIM_OC_ConfigChannel(htim, &sConfig, TIM_CHANNEL_2) != HAL_OK)
{
/* Configuration Error */
Error_Handler();
}
}
static void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
/* Enable Power Control clock */
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/* Enable HSI Oscillator and activate PLL with HSI as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 0x10;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 400;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
this is msp.c
void HAL_TIM_Encoder_MspInit(TIM_HandleTypeDef *htim)
{
GPIO_InitTypeDef GPIO_InitStruct;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* TIM1 Peripheral clock enable */
__HAL_RCC_TIM1_CLK_ENABLE();
/* Enable GPIO Channels Clock */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
/*##-2- Configure I/Os #####################################################*/
/* Common configuration for all channels */
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF1_TIM1;
/* Channel 1 configuration */
GPIO_InitStruct.Pin = GPIO_PIN_8;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Channel 2 configuration */
GPIO_InitStruct.Pin = GPIO_PIN_11;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
}
when i set TIM_Encoder_MspInit, tim9(PE5 and PE6) to be encoder timer then i just read 0, and tim5 also, by the way now i use tim1(PA8 and PE11), and when change to (PA8 and PA9) then can not work, change to (PE11 and PE9) can also work, i dont know why.