Skip to main content
Associate
April 24, 2025
Solved

STM32F407VG to PC Communication via CAN – USB-to-CAN Adapter Recommendation

  • April 24, 2025
  • 1 reply
  • 856 views

Hello,

I’m working with the STM32F407VG microcontroller and I want to establish communication between the PC and the board using CAN protocol. Which USB-to-CAN adapter is recommended for CAN communication with Board.

[STM32 Board] --- [USB-to-CAN Adapter] --- [PC]

Best answer by mƎALLEm

First of all you need to establish a complete CAN bus with at least two CAN nodes. Then, in your case, the first node contains STM32F407 MCU with a CAN transceiver + a terminating resistor of 120 ohm and the second node a CAN/USB adapter on which you need to enable an internal 120ohm terminating resistor.

This is a minimal CAN bus structure:

https://community.st.com/t5/stm32-mcus/stm32-fdcan-running-at-8-mb-s-on-nucleo-boards/ta-p/730281?lightbox-message-images-730281=90488iD4EA082CEF3B11D9

I cannot give a recommendation for an USB-to-CAN adapter. But I can give an example: https://www.waveshare.com/usb-can-a.htm

But this is not a recommendation it's up to you to decide as this is not an ST product.

Meanwhile, from the microcontroller side, you need to add a transceiver for example what was used on several ST boards: SN65HVD230.

CAN communication example is provided here.

If you are not familiar with the CAN bus you need to study it before going ahead with using as communication medium.

Hope that helps.

 

1 reply

mƎALLEm
ST Technical Moderator
April 24, 2025

Hello @Loganathan and welcome to the ST community,

So where is the question? and which board are you using for STM32F407VG microcontroller?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate
April 24, 2025

Hi,

How to establish CAN communication between STM32F407VG and PC via USB-to-CAN adapter? Which USB-to-CAN adapter do you recommend for stable and compatible CAN communication between the STM32F407VG board and a Windows PC?

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 24, 2025

First of all you need to establish a complete CAN bus with at least two CAN nodes. Then, in your case, the first node contains STM32F407 MCU with a CAN transceiver + a terminating resistor of 120 ohm and the second node a CAN/USB adapter on which you need to enable an internal 120ohm terminating resistor.

This is a minimal CAN bus structure:

https://community.st.com/t5/stm32-mcus/stm32-fdcan-running-at-8-mb-s-on-nucleo-boards/ta-p/730281?lightbox-message-images-730281=90488iD4EA082CEF3B11D9

I cannot give a recommendation for an USB-to-CAN adapter. But I can give an example: https://www.waveshare.com/usb-can-a.htm

But this is not a recommendation it's up to you to decide as this is not an ST product.

Meanwhile, from the microcontroller side, you need to add a transceiver for example what was used on several ST boards: SN65HVD230.

CAN communication example is provided here.

If you are not familiar with the CAN bus you need to study it before going ahead with using as communication medium.

Hope that helps.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.